This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
cc2540可以组微微网吗?怎么组呢?
蓝牙节点组网中,只能存在一个主节点(Central)和多个从节点(Peripheral),从节点是发出信号者,主节点是扫描且发起连接者。
dirtwillfly,
可以的,一个central连接多个peripheral设备。
理论上只能同时一对7吧。
我是这样理解组网的:
可不可以让从设备需要通信的时候,让自己广播,主机扫到就连接,然后通信。通信完毕就断开。
这样1个主机可以搞很多个从机了,但是不能同时连接7个以上。
fordream,
你的想法非常好,这个方式对于功耗什么来说都很好。
BLE 不像传统蓝牙只能有7个,没有规定具体能连几个。