This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC256x MSP430 Bluetopia SDK\v1.4 R1基础上改,实现 HFP(语音免提) + BLE(传输控制数据 和传感数据)



在CC256x MSP430 Bluetopia SDK\v1.4 R1基础上改,实现 HFP(语音免提)   +   BLE(传输控制数据 和传感数据)。在哪一个例子上面改最方便?因为在430平台上,TI已经有做好了以下例子:

SPP Demo

  • This application shows how to utilize the SPP module and also how handle the different callback events. The application can be used to interface with a remote SPP Client or Server.

SPP + SPPLE Demo

  • This application shows how to utilize Low Energy (LE) and the GATT profile. This sample emulates using SPP over LE using the GATT Profile. This sample acts as a LE Master and LE Slave.
  • This application also shows how to utilize the SPP module and how to handle the different SPP callback events. This will act as either a SPP Server or SPP Client and exposes the same command set for SPP as the SPPDemo.

ANP Demo

  • This application shows how to utilize Low Energy (LE) and the GATT profile. This sample implements the Alert Notification Profile (ANP) using the GATT profile. This sample acts as a LE Master and LE Slave.

HRP Demo

  • This application shows how to utilize Low Energy (LE) and the GATT profile. This sample implements the Heart Rate Monitoring Profile (HRP) using the GATT profile. This sample acts as a LE Master and LE Slave.

HTP Demo

  • This application shows how to utilize Low Energy (LE) and the GATT profile. This sample implements the Health Thermometer Profile (HTP) using the GATT profile. This sample acts as a LE Master and LE Slave.

PASP Demo

  • This application shows how to utilize Low Energy (LE) and the GATT profile. This sample implements the Phone Alert Status Profile (PASP) using the GATT profile. This sample acts as a LE Master and LE Slave.