我使用的是KeyFob,想要使能usart0 alt2也就是 p1.4,p1.5为串口与pc通讯不知道如何设置,另外,不知道HAL_UART_DMA = 1,2,区别仔细看了下,感觉就是alt1与alt2的选择。但是定义为2也是不能使能uart0,alt2这个端口。
另外以下这些变量是什么意思呢?具体能用来做什么?
1.gapCentralRoleIRK
2.gapCentralRoleSRK
3.gapCentralRoleSignCounter
4.IO_CAPABILITIES;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用的是KeyFob,想要使能usart0 alt2也就是 p1.4,p1.5为串口与pc通讯不知道如何设置,另外,不知道HAL_UART_DMA = 1,2,区别仔细看了下,感觉就是alt1与alt2的选择。但是定义为2也是不能使能uart0,alt2这个端口。
另外以下这些变量是什么意思呢?具体能用来做什么?
1.gapCentralRoleIRK
2.gapCentralRoleSRK
3.gapCentralRoleSignCounter
4.IO_CAPABILITIES;
英文手册USART 0 and USART 1 are each configurable as either an SPI master/slave or a UART. They provide double
buffering on both RX and TX and hardware flow control and are thus well suited to high-throughput full-duplex
applications. Each USART has its own high-precision baud-rate generator, thus leaving the ordinary timers free
for other uses. When configured as SPI slaves, the USARTs sample the input signal using SCK directly instead
of using some oversampling scheme, and are thus well-suited for high data rates.
下面这段代码是官方的串口初始化函数,如果这样设置并且HAL_UART_DMA = 1 的时候,串口0 的p02,p03能正常使用
但是我想使用串口0 的p1口,也就是alt2功能 注释掉的代码就是相应的寄存器配置,但是 仍然无法使用串口0的p1口。
我发现当HAL_UART_DMA = 2时,就是跟配置串口0alt2的代码是一样的。只是不知道那句官方注释是不是对的。
但是串口0的p1口不能使用。不知道是不是少了什么。
static void HalUARTInitDMA(void)
{
halDMADesc_t *ch;
#if (HAL_UART_DMA == 1)
PERCFG &= ~HAL_UART_PERCFG_BIT; // Set UART0 I/O to Alt. 1 location on P0. 这里官方注释使用uart0 的 alt 1 p0端口 可以理解
#else
PERCFG |= HAL_UART_PERCFG_BIT; // Set UART1 I/O to Alt. 2 location on P1.问题1:这里使能uart1 的 alt2 使用p1口的uart1??
// PERCFG = PERCFG | 0x01; //usart 0 alt 2 location
#endif
PxSEL |= HAL_UART_Px_SEL; // Enable Peripheral control of Rx/Tx on Px.
//P1SEL = P1SEL | 0x30; //p1 function peripheral function.
UxCSR = CSR_MODE; // Mode is UART Mode.
//U1CSR = U1CSR | 0xC0;// Mode is UART Mode.
UxUCR = UCR_FLUSH; // Flush it.
//U1UCR = 0x80;//// Flush it.
// P2SEL = P2SEL & 0xBF; //usart 0 has priority
// P2DIR = P2DIR & 0x3F;//1st priority usart0
P2DIR &= ~P2DIR_PRIPO;
P2DIR |= HAL_UART_PRIPO;
以下代码还有不过好像跟串口无关
……
}
/***********************************************************************************
Filename: uart_poll.c
Description: This example sends/receives data on UART0, using polling method.
Comments: To execute this example, compile one SmartRF05EB unit as transmitter,
by activating the UART_TST_MODE_TX definition, then compile another
unit as receiver, by activating the UART_TST_MODE_RX definition.
Pressing S1 makes the transmitter send its allocated uartTxBuffer[]
to the receiver. The transferred data will arrive at uartRxBuffer[]
and can be verified using the debugger.
Note: Once the UART receiver has been enabled (U0CSR.RE = 1) it will
automatically trigger data reception as soon the Start bit is
detected. The transmitter I/O should therefore be configured
before the receiver, such that potential pin toggling (during
I/O configuration of the transmitter) does not trigger data
reception at the receiver side. Also, remember to use common
ground for the TX unit and RX unit!
***********************************************************************************/
/***********************************************************************************
* INCLUDES
*/
#include <hal_types.h>
// Include Name definitions of individual bits and bit-fields in the CC254x device registers.
#include <ioCC254x_bitdef.h>
// Include device specific file
#if (chip==2541)
#include "ioCC2541.h"
#elif (chip==2543)
#include "ioCC2543.h"
#elif (chip==2544)
#include "ioCC2544.h"
#warning "The CC2544Dongle is not supported for this software example."
#warning "The definitions for CC2544 in the code illustrate how to set up an SPI interface."
#elif (chip==2545)
#include "ioCC2545.h"
#else
#error "Chip not supported!"
#endif
/***********************************************************************************
* CONSTANTS
*/
// Define size of allocated UART RX/TX buffer (just an example).
#define SIZE_OF_UART_RX_BUFFER 50
#define SIZE_OF_UART_TX_BUFFER SIZE_OF_UART_RX_BUFFER
// UART test characters.
#define UART_TEST_DATA "Texas Instruments LPRF!"
// Test definitions.
#define UART_TST_MODE_RX
//#define UART_TST_MODE_TX
// Baudrate = 57.6 kbps (U0BAUD.BAUD_M = 216, U0GCR.BAUD_E = 10), given 32 MHz system clock.
#define UART_BAUD_M 216
#define UART_BAUD_E 10
/***********************************************************************************
* LOCAL VARIABLES
*/
// Buffer for UART RX/TX.
static uint8 __xdata uartRxBuffer[SIZE_OF_UART_RX_BUFFER];
static uint8 __xdata uartTxBuffer[SIZE_OF_UART_TX_BUFFER] = UART_TEST_DATA;
// Prototype for local functions.
void uart0Send(uint8* uartTxBuf, uint16 uartTxBufLength);
void uart0Receive(uint8* uartRxBuf, uint16 uartRxBufLength);
/***********************************************************************************
* @fn main
*
* @brief Send/receive data on UART0, using polling.
*
* @param void
*
* @return void
*/
void main (void)
{
/****************************************************************************
* Clock setup
* See basic software example "clk_xosc_cc254x"
*/
// Set system clock source to HS XOSC, with no pre-scaling.
CLKCONCMD = (CLKCONCMD & ~(CLKCON_OSC | CLKCON_CLKSPD)) | CLKCON_CLKSPD_32M;
// Wait until clock source has changed.
while (CLKCONSTA & CLKCON_OSC);
/* Note the 32 kHz RCOSC starts calibrating, if not disabled. */
/***************************************************************************
* Setup I/O ports
*
* Port and pins used by USART0 operating in UART-mode, at the Alternative 1
* location are:
* RX : P0_2
* TX : P0_3
* CT/CTS : P0_4
* RT/RTS : P0_5
*
* These pins must be set to function as peripheral I/O to be used by UART0.
* The TX pin on the transmitter must be connected to the RX pin on the receiver.
* If enabling hardware flow control (U0UCR.FLOW = 1) the CT/CTS (Clear-To-Send)
* on the transmitter must be connected to the RS/RTS (Ready-To-Send) pin on the
* receiver.
*/
#if (chip==2541 || chip==2543 || chip==2545)
// Configure USART0 for Alternative 1 => Port P0 (PERCFG.U0CFG = 0).
PERCFG = (PERCFG & ~PERCFG_U0CFG) | PERCFG_U0CFG_ALT1;
#endif
#if (chip==2541)
// Give priority to USART 0 over Timer 1 for port 0 pins.
P2DIR &= P2DIR_PRIP0_USART0;
#elif (chip==2543 || chip==2545)
// Give priority to USART 0 over Timer 1 for port 0 pins.
PPRI &= ~PPRI_PRI0P0;
#endif
#if (chip==2541 || chip==2543 || chip==2545)
// Set pins 2, 3 and 5 as peripheral I/O and pin 4 as GPIO output.
P0SEL |= BIT5 | BIT4 | BIT3 | BIT2;
#elif (chip==2544)
// Set pins 1, 2 and 3 as peripheral I/O and pin 0 as GPIO output.
P0SEL0 = 0x11; // Map P0_0 and P0_1 as UASRT0.
P0SEL1 = 0x11; // Map P0_3 and P0_2 as UASRT0.
#endif
#if (chip==2541 || chip==2543 || chip==2545)
// Initialize P0_1 for SRF05EB S1 button.
P0SEL &= ~BIT1; // Function as General Purpose I/O.
P0DIR &= ~BIT1; // Input.
#elif (chip==2544)
// Initialize P0_1 for SRF05EB S1 button.
P0SEL0 &= ~P0SEL0_SELP0_1;// Function as General Purpose I/O.
PDIR &= ~PDIR_DIRP0_1; // Input.
#endif
/***************************************************************************
* Configure UART
*
*/
// Initialise bitrate = 57.6 kbps.
U0BAUD = UART_BAUD_M;
U0GCR = (U0GCR & ~U0GCR_BAUD_E) | UART_BAUD_E;
// Initialise UART protocol (start/stop bit, data bits, parity, etc.):
// USART mode = UART (U0CSR.MODE = 1)
U0CSR |= U0CSR_MODE;
// Start bit level = low => Idle level = high (U0UCR.START = 0).
U0UCR &= ~U0UCR_START;
// Stop bit level = high (U0UCR.STOP = 1).
U0UCR |= U0UCR_STOP;
// Number of stop bits = 1 (U0UCR.SPB = 0).
U0UCR &= ~U0UCR_SPB;
// Parity = disabled (U0UCR.PARITY = 0).
U0UCR &= ~U0UCR_PARITY;
// 9-bit data enable = 8 bits transfer (U0UCR.BIT9 = 0).
U0UCR &= ~U0UCR_BIT9;
// Level of bit 9 = 0 (U0UCR.D9 = 0), used when U0UCR.BIT9 = 1.
// Level of bit 9 = 1 (U0UCR.D9 = 1), used when U0UCR.BIT9 = 1.
// Parity = Even (U0UCR.D9 = 0), used when U0UCR.PARITY = 1.
// Parity = Odd (U0UCR.D9 = 1), used when U0UCR.PARITY = 1.
U0UCR &= ~U0UCR_D9;
// Flow control = disabled (U0UCR.FLOW = 0).
U0UCR &= ~U0UCR_FLOW;
// Bit order = LSB first (U0GCR.ORDER = 0).
U0GCR &= ~U0GCR_ORDER;
/***************************************************************************
* Transfer UART data
*/
while(1)
{
#ifdef UART_TST_MODE_RX
uart0Receive(uartRxBuffer, SIZE_OF_UART_RX_BUFFER);
#else
// If SRF05EB S1 button is pressed (S1 high when pushed).
if (P0 & BIT1)
{
uart0Send(uartTxBuffer, SIZE_OF_UART_TX_BUFFER);
}
#endif
}
}
/***********************************************************************************
* LOCAL FUNCTIONS
*/
/***********************************************************************************
* @fn uart0Send
*
* @brief Function which sends a requested number of bytes on UART0
*
* @param uint8* uartTxBuf - address of allocated UART TX buffer
* uint16 uartTxBufLength - size of allocated UART TX buffer
*
* @return void
*/
void uart0Send(uint8* uartTxBuf, uint16 uartTxBufLength)
{
uint16 uartTxIndex;
// Clear any pending TX interrupt request (set U0CSR.TX_BYTE = 0).
U0CSR &= ~U0CSR_TX_BYTE;
// Loop: send each UART0 sample on the UART0 TX line.
for (uartTxIndex = 0; uartTxIndex < uartTxBufLength; uartTxIndex++)
{
U0DBUF = uartTxBuf[uartTxIndex];
while(! (U0CSR & U0CSR_TX_BYTE) );
U0CSR &= ~U0CSR_TX_BYTE;
}
}
/***********************************************************************************
* @fn uart0Receive
*
* @brief Function which receives a requested number of bytes on UART0
*
* @param uint8* uartRxBuf - address of allocated UART RX buffer
* uint16 uartRxBufLength - size of allocated UART RX buffer
*
* @return void
*/
void uart0Receive(uint8* uartRxBuf, uint16 uartRxBufLength)
{
uint16 uartRxIndex;
// Enable UART0 RX (U0CSR.RE = 1).
U0CSR |= U0CSR_RE;
// Clear any pending RX interrupt request (set U0CSR.RX_BYTE = 0).
U0CSR &= ~U0CSR_RX_BYTE;
// Loop: receive each UART0 sample from the UART0 RX line.
for (uartRxIndex = 0; uartRxIndex < uartRxBufLength; uartRxIndex++)
{
// Wait until data received (U0CSR.RX_BYTE = 1).
while( !(U0CSR & U0CSR_RX_BYTE) );
// Read UART0 RX buffer.
uartRxBuf[uartRxIndex] = U0DBUF;
}
}
/***********************************************************************************
Copyright 2012 Texas Instruments Incorporated. All rights reserved.
IMPORTANT: Your use of this Software is limited to those specific rights
granted under the terms of a software license agreement between the user
who downloaded the software, his/her employer (which must be your employer)
and Texas Instruments Incorporated (the "License"). You may not use this
Software unless you agree to abide by the terms of the License. The License
limits your use, and you acknowledge, that the Software may not be modified,
copied or distributed unless embedded on a Texas Instruments microcontroller
or used solely and exclusively in conjunction with a Texas Instruments radio
frequency transceiver, which is integrated into your product. Other than for
the foregoing purpose, you may not use, reproduce, copy, prepare derivative
works of, modify, distribute, perform, display or sell this Software and/or
its documentation for any purpose.
YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
PROVIDED 揂S IS?WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
(INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
Should you have any questions regarding your right to use this Software,
contact Texas Instruments Incorporated at www.TI.com.
***********************************************************************************/