请问这部分内容的从机的哪部分函数实现了?想在这里添加查询是否有数据需要发送的函数。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
cg,
这部分是通过connection update request 实现的。你可以看一下初始化函数里面的下面这段代码:
uint8 enable_update_request = DEFAULT_ENABLE_UPDATE_REQUEST;
uint16 desired_min_interval = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
uint16 desired_max_interval = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
uint16 desired_slave_latency = DEFAULT_DESIRED_SLAVE_LATENCY;
uint16 desired_conn_timeout = DEFAULT_DESIRED_CONN_TIMEOUT;
// Set the GAP Role Parameters
GAPRole_SetParameter( GAPROLE_ADVERT_ENABLED, sizeof( uint8 ), &initial_advertising_enable );
GAPRole_SetParameter( GAPROLE_ADVERT_OFF_TIME, sizeof( uint16 ), &gapRole_AdvertOffTime );
GAPRole_SetParameter( GAPROLE_SCAN_RSP_DATA, sizeof ( scanRspData ), scanRspData );
GAPRole_SetParameter( GAPROLE_ADVERT_DATA, sizeof( advertData ), advertData );
GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_ENABLE, sizeof( uint8 ), &enable_update_request );
GAPRole_SetParameter( GAPROLE_MIN_CONN_INTERVAL, sizeof( uint16 ), &desired_min_interval );
GAPRole_SetParameter( GAPROLE_MAX_CONN_INTERVAL, sizeof( uint16 ), &desired_max_interval );
GAPRole_SetParameter( GAPROLE_SLAVE_LATENCY, sizeof( uint16 ), &desired_slave_latency );
GAPRole_SetParameter( GAPROLE_TIMEOUT_MULTIPLIER, sizeof( uint16 ), &desired_conn_timeout );
具体操作是由link layer做的,这部分代码是以库的形式存在,你看不到。
Yan
// Minimum connection interval (units of 1.25ms, 80=100ms) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 800
// Maximum connection interval (units of 1.25ms, 800=1000ms) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 800
// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_DESIRED_SLAVE_LATENCY 50
// Supervision timeout value (units of 10ms, 1000=10s) if automatic parameter update request is enabled
#define DEFAULT_DESIRED_CONN_TIMEOUT 1000
// Whether to enable automatic parameter update request when a connection is formed
#define DEFAULT_ENABLE_UPDATE_REQUEST TRUE
我把参数改成这个情况,按理来说超过10s后蓝牙应该会断开连接,但实际上没有断开,具体原因是什么呢?我知道从机是没有更新参数的功能,只有发送请求,是不是因为请求没有被主机相应?如果是这样,怎样才能让主机相应参数更新的请求?
ViKi
从机设置中,是以下参数设置CONN_INTERVAL、SLAVE_LATENCY这些,是不是设置了这些参数,主机就会响应?没发现从机中有GAPRole_SendUpdateParam( )发这个函数的调用?
GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_ENABLE, sizeof( uint8 ), &enable_update_request );
GAPRole_SetParameter( GAPROLE_MIN_CONN_INTERVAL, sizeof( uint16 ), &desired_min_interval );
GAPRole_SetParameter( GAPROLE_MAX_CONN_INTERVAL, sizeof( uint16 ), &desired_max_interval );
GAPRole_SetParameter( GAPROLE_SLAVE_LATENCY, sizeof( uint16 ), &desired_slave_latency );
GAPRole_SetParameter( GAPROLE_TIMEOUT_MULTIPLIER, sizeof( uint16 ), &desired_conn_timeout );