This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc256x spple链路与a2dp链路是否能并存

Other Parts Discussed in Thread: CC2564

iphone已经连接上cc256x做a2dp音乐播放,如果这台iphone还想通过spple来控制cc256x ,是否可行。

也就是说cc256x的双模式是否可以是BR/EDR + LE slave ?

  • wang,

    是的,完全可以!

    两路并存,一起工作,这是CC2564作为双模蓝牙的基本功能:)

  • 我想把协议方面再明确一下,BR/EDR( a2dp + avrcp + spp)  +  spple(le slave)  与同一台iphone设备进行连接,可以从cc2564听音乐,并且接受iphone 的控制(一些开关量传输),同时还可以从其它非4.0蓝牙设备通过BR/EDR的spp连接来控制(一些开关量传输)。

    因为我了解到另一款CSR的蓝牙双模芯片只能做BR/EDR + le master 双链接,因此有疑问。

    如果可行的话,我们要切换到cc2564平台。

    谢谢。

  • wang,

    2564可以做到BR/EDR 当 master, LE 当slave。

    2564的LE 属性支持master 和 slave 模式。

  • Hi  Wang

    可以的,我们已经有相关产品,如需要演示Demo,可以与我联系:kevin.zhou@wi-linktech.com,维霖通(上海)是TI大陆地区蓝牙合作伙伴,你可以在TI网站上中国合作伙伴中找到我们。