请教CC245x ble配对绑定central端程序要如何设置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
xiwen,
在void SimpleBLECentral_Init( ) 中,
有
// Setup the GAP Bond Manager
{
uint32 passkey = DEFAULT_PASSCODE;
uint8 pairMode = DEFAULT_PAIRING_MODE;
uint8 mitm = DEFAULT_MITM_MODE;
uint8 ioCap = DEFAULT_IO_CAPABILITIES;
uint8 bonding = DEFAULT_BONDING_MODE;
GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof( uint32 ), &passkey );
GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof( uint8 ), &pairMode );
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof( uint8 ), &mitm );
GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof( uint8 ), &ioCap );
GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof( uint8 ), &bonding );
}
这里就是所有的配对绑定配置。
您好,感谢您的回复,我想实现的功能是central端和peripheral端有一个身份的验证,只有passkey一致才能配对成功,根据您的回复主机端设置为:
// Setup the GAP Bond Manager
{
uint32 passkey = DEFAULT_PASSCODE;
uint8 pairMode = DEFAULT_PAIRING_MODE;
uint8 mitm = DEFAULT_MITM_MODE;
uint8 ioCap = DEFAULT_IO_CAPABILITIES;
uint8 bonding = DEFAULT_BONDING_MODE;
GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof( uint32 ), &passkey );
GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof( uint8 ), &pairMode );
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof( uint8 ), &mitm );
GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof( uint8 ), &ioCap );
GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof( uint8 ), &bonding );
}
从机端设置为
// Setup the GAP Bond Manager
{
uint32 passkey = 0; // passkey "000000"
//uint8 pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
uint8 pairMode = GAPBOND_PAIRING_MODE_INITIATE;
uint8 mitm = TRUE;
uint8 ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
uint8 bonding = TRUE;
GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof ( uint32 ), &passkey );
GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof ( uint8 ), &pairMode );
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof ( uint8 ), &mitm );
GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof ( uint8 ), &ioCap );
GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof ( uint8 ), &bonding );
}
这样设置的话是不是主机端和从机端的passkey相同是才能绑定成功,如果不能实现,有没有其他的方法,谢谢!