char5原来是只读的
我把他改成了static uint8 simpleProfileChar5Props = GATT_PROP_READ | GATT_PROP_WRITE; ////可读可写
同时
// Characteristic Value 5
{
{ ATT_BT_UUID_SIZE, simpleProfilechar5UUID },
GATT_PERMIT_AUTHEN_READ | GATT_PERMIT_AUTHEN_WRITE, /////认证后可读可写
0,
simpleProfileChar5
},
然后我在simpleProfile_WriteAttrCB函数里面打了一个断点,每当我写char5的时候,断点停下的时候会有如下的打印
The stack 'XdataStack' is filled to 100% (640 bytes used out of 640). The warning threshold is set to 90.%
这是怎么回事啊,但如果不管它,貌似char5写进去的值也生效了
但如果我把GATT_PERMIT_AUTHEN_READ | GATT_PERMIT_AUTHEN_WRITE 改成GATT_PERMIT_READ | GATT_PERMIT_WRITE就没这个问题了
好奇怪