This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

讨论,移植SimpleBLECentral程序,把2540 usb dongle变成主机(不连接电脑)?

Other Parts Discussed in Thread: CC2540

实现扫描和链接!

2540 usb dongle只有两个按键,p1.2,p1.3.

 

  • /**************************************************************************************************
      Filename:       hal_key.c
      Revised:        $Date: 2013-09-20 11:53:10 -0700 (Fri, 20 Sep 2013) $
      Revision:       $Revision: 35401 $

      Description:    This file contains the interface to the HAL KEY Service.


      Copyright 2006-2013 Texas Instruments Incorporated. All rights reserved.

      IMPORTANT: Your use of this Software is limited to those specific rights
      granted under the terms of a software license agreement between the user
      who downloaded the software, his/her employer (which must be your employer)
      and Texas Instruments Incorporated (the "License").  You may not use this
      Software unless you agree to abide by the terms of the License. The License
      limits your use, and you acknowledge, that the Software may not be modified,
      copied or distributed unless embedded on a Texas Instruments microcontroller
      or used solely and exclusively in conjunction with a Texas Instruments radio
      frequency transceiver, which is integrated into your product.  Other than for
      the foregoing purpose, you may not use, reproduce, copy, prepare derivative
      works of, modify, distribute, perform, display or sell this Software and/or
      its documentation for any purpose.

      YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
      PROVIDED 揂S IS?WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
      INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
      NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
      TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
      NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
      LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
      INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
      OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
      OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
      (INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.

      Should you have any questions regarding your right to use this Software,
      contact Texas Instruments Incorporated at www.TI.com.
    **************************************************************************************************/
    /*********************************************************************
     NOTE: If polling is used, the hal_driver task schedules the KeyRead()
           to occur every 100ms.  This should be long enough to naturally
           debounce the keys.  The KeyRead() function remembers the key
           state of the previous poll and will only return a non-zero
           value if the key state changes.

     NOTE: If interrupts are used, the KeyRead() function is scheduled
           25ms after the interrupt occurs by the ISR.  This delay is used
           for key debouncing.  The ISR disables any further Key interrupt
           until KeyRead() is executed.  KeyRead() will re-enable Key
           interrupts after executing.  Unlike polling, when interrupts
           are enabled, the previous key state is not remembered.  This
           means that KeyRead() will return the current state of the keys
           (not a change in state of the keys).

     NOTE: If interrupts are used, the KeyRead() fucntion is scheduled by
           the ISR.  Therefore, the joystick movements will only be detected
           during a pushbutton interrupt caused by S1 or the center joystick
           pushbutton.

     NOTE: When a switch like S1 is pushed, the S1 signal goes from a normally
           high state to a low state.  This transition is typically clean.  The
           duration of the low state is around 200ms.  When the signal returns
           to the high state, there is a high likelihood of signal bounce, which
           causes a unwanted interrupts.  Normally, we would set the interrupt
           edge to falling edge to generate an interrupt when S1 is pushed, but
           because of the signal bounce, it is better to set the edge to rising
           edge to generate an interrupt when S1 is released.  The debounce logic
           can then filter out the signal bounce.  The result is that we typically
           get only 1 interrupt per button push.  This mechanism is not totally
           foolproof because occasionally, signal bound occurs during the falling
           edge as well.  A similar mechanism is used to handle the joystick
           pushbutton on the DB.  For the EB, we do not have independent control
           of the interrupt edge for the S1 and center joystick pushbutton.  As
           a result, only one or the other pushbuttons work reasonably well with
           interrupts.  The default is the make the S1 switch on the EB work more
           reliably.

    *********************************************************************/

    /**************************************************************************************************
     *                                            INCLUDES
     **************************************************************************************************/
    #include "hal_mcu.h"
    #include "hal_defs.h"
    #include "hal_types.h"
    #include "hal_drivers.h"
    #include "hal_adc.h"
    #include "hal_key.h"
    #include "osal.h"

    #if (defined HAL_KEY) && (HAL_KEY == TRUE)

    /**************************************************************************************************
     *                                            CONSTANTS
     **************************************************************************************************/
    #define HAL_KEY_RISING_EDGE   0
    #define HAL_KEY_FALLING_EDGE  1

    #define HAL_KEY_DEBOUNCE_VALUE  25

    /* CPU port interrupt */
    #define HAL_KEY_CPU_PORT_0_IF P0IF
    #define HAL_KEY_CPU_PORT_2_IF P2IF

    #if defined ( CC2540_MINIDK )
    /* SW_1 is at P0.0 */
    #define HAL_KEY_SW_1_PORT   P0
    #define HAL_KEY_SW_1_BIT    BV(0)
    #define HAL_KEY_SW_1_SEL    P0SEL
    #define HAL_KEY_SW_1_DIR    P0DIR

    /* SW_2 is at P0.1 */
    #define HAL_KEY_SW_2_PORT   P0
    #define HAL_KEY_SW_2_BIT    BV(1)
    #define HAL_KEY_SW_2_SEL    P0SEL
    #define HAL_KEY_SW_2_DIR    P0DIR

    #define HAL_KEY_SW_1_IEN      IEN1  /* CPU interrupt mask register */
    #define HAL_KEY_SW_1_ICTL     P0IEN /* Port Interrupt Control register */
    #define HAL_KEY_SW_1_ICTLBIT  BV(0) /* P0IEN - P0.0 enable/disable bit */
    #define HAL_KEY_SW_1_IENBIT   BV(5) /* Mask bit for all of Port_0 */

    #define HAL_KEY_SW_1_PXIFG    P0IFG /* Interrupt flag at source */
    #define HAL_KEY_SW_2_IEN      IEN1  /* CPU interrupt mask register */
    #define HAL_KEY_SW_2_ICTL     P0IEN /* Port Interrupt Control register */
    #define HAL_KEY_SW_2_ICTLBIT  BV(1) /* P0IEN - P0.1 enable/disable bit */
    #define HAL_KEY_SW_2_IENBIT   BV(5) /* Mask bit for all of Port_0 */
    #define HAL_KEY_SW_2_PXIFG    P0IFG /* Interrupt flag at source */

    #define HAL_KEY_SW_1_EDGEBIT  BV(0)

    #else

    /* SW_6 is at P0.1 */
    #define HAL_KEY_SW_6_PORT   P0
    #define HAL_KEY_SW_6_BIT    BV(1)
    #define HAL_KEY_SW_6_SEL    P0SEL
    #define HAL_KEY_SW_6_DIR    P0DIR

    /* edge interrupt */
    #define HAL_KEY_SW_6_EDGEBIT  BV(0)
    #define HAL_KEY_SW_6_EDGE     HAL_KEY_FALLING_EDGE

    /* SW_6 interrupts */
    #define HAL_KEY_SW_6_IEN      IEN1  /* CPU interrupt mask register */
    #define HAL_KEY_SW_6_IENBIT   BV(5) /* Mask bit for all of Port_0 */
    #define HAL_KEY_SW_6_ICTL     P0IEN /* Port Interrupt Control register */
    #define HAL_KEY_SW_6_ICTLBIT  BV(1) /* P0IEN - P0.1 enable/disable bit */
    #define HAL_KEY_SW_6_PXIFG    P0IFG /* Interrupt flag at source */

    /* Joy stick move at P2.0 */
    #define HAL_KEY_JOY_MOVE_PORT   P2
    #define HAL_KEY_JOY_MOVE_BIT    BV(0)
    #define HAL_KEY_JOY_MOVE_SEL    P2SEL
    #define HAL_KEY_JOY_MOVE_DIR    P2DIR

    /* edge interrupt */
    #define HAL_KEY_JOY_MOVE_EDGEBIT  BV(3)
    #define HAL_KEY_JOY_MOVE_EDGE     HAL_KEY_FALLING_EDGE

    /* Joy move interrupts */
    #define HAL_KEY_JOY_MOVE_IEN      IEN2  /* CPU interrupt mask register */
    #define HAL_KEY_JOY_MOVE_IENBIT   BV(1) /* Mask bit for all of Port_2 */
    #define HAL_KEY_JOY_MOVE_ICTL     P2IEN /* Port Interrupt Control register */
    #define HAL_KEY_JOY_MOVE_ICTLBIT  BV(0) /* P2IENL - P2.0<->P2.3 enable/disable bit */
    #define HAL_KEY_JOY_MOVE_PXIFG    P2IFG /* Interrupt flag at source */

    #define HAL_KEY_JOY_CHN   HAL_ADC_CHANNEL_6

    #endif

    /**************************************************************************************************
     *                                            TYPEDEFS
     **************************************************************************************************/


    /**************************************************************************************************
     *                                        GLOBAL VARIABLES
     **************************************************************************************************/
    static uint8 halKeySavedKeys;     /* used to store previous key state in polling mode */
    static halKeyCBack_t pHalKeyProcessFunction;
    static uint8 HalKeyConfigured;
    bool Hal_KeyIntEnable;            /* interrupt enable/disable flag */

    /**************************************************************************************************
     *                                        FUNCTIONS - Local
     **************************************************************************************************/
    void halProcessKeyInterrupt(void);
    uint8 halGetJoyKeyInput(void);

     

    /**************************************************************************************************
     *                                        FUNCTIONS - API
     **************************************************************************************************/


    /**************************************************************************************************
     * @fn      HalKeyInit
     *
     * @brief   Initilize Key Service
     *
     * @param   none
     *
     * @return  None
     **************************************************************************************************/
    void HalKeyInit( void )
    {
      halKeySavedKeys = 0;  // Initialize previous key to 0.

    #if defined ( CC2540_MINIDK )
      HAL_KEY_SW_1_SEL &= ~(HAL_KEY_SW_1_BIT);    /* Set pin function to GPIO */
      HAL_KEY_SW_1_DIR &= ~(HAL_KEY_SW_1_BIT);    /* Set pin direction to Input */
      HAL_KEY_SW_2_SEL &= ~(HAL_KEY_SW_2_BIT);    /* Set pin function to GPIO */
      HAL_KEY_SW_2_DIR &= ~(HAL_KEY_SW_2_BIT);    /* Set pin direction to Input */
    #else
      HAL_KEY_SW_6_SEL &= ~(HAL_KEY_SW_6_BIT);    /* Set pin function to GPIO */
      HAL_KEY_SW_6_DIR &= ~(HAL_KEY_SW_6_BIT);    /* Set pin direction to Input */
      HAL_KEY_JOY_MOVE_SEL &= ~(HAL_KEY_JOY_MOVE_BIT); /* Set pin function to GPIO */
      HAL_KEY_JOY_MOVE_DIR &= ~(HAL_KEY_JOY_MOVE_BIT); /* Set pin direction to Input */

      P2INP |= PUSH2_BV;  /* Configure GPIO tri-state. */
    #endif

      /* Initialize callback function */
      pHalKeyProcessFunction  = NULL;

      /* Start with key is not configured */
      HalKeyConfigured = FALSE;

    #if defined ( CC2540_MINIDK )
      /* Rising/Falling edge configuratinn */
      PICTL |= HAL_KEY_SW_1_EDGEBIT;   /* Set the edge bit to set falling edge to give int */
      HAL_KEY_SW_1_IEN |= ( HAL_KEY_SW_1_IENBIT | HAL_KEY_SW_2_IENBIT );   /* enable CPU interrupt */
    #endif
    }


    /**************************************************************************************************
     * @fn      HalKeyConfig
     *
     * @brief   Configure the Key serivce
     *
     * @param   interruptEnable - TRUE/FALSE, enable/disable interrupt
     *          cback - pointer to the CallBack function
     *
     * @return  None
     **************************************************************************************************/
    void HalKeyConfig (bool interruptEnable, halKeyCBack_t cback)
    {
      /* Enable/Disable Interrupt or */
      Hal_KeyIntEnable = interruptEnable;

      /* Register the callback fucntion */
      pHalKeyProcessFunction = cback;

      /* Determine if interrupt is enable or not */
      if (Hal_KeyIntEnable)
      {
    #if defined ( CC2540_MINIDK )
        HAL_KEY_SW_1_ICTL |= HAL_KEY_SW_1_ICTLBIT; /* enable interrupt generation at port */   
        HAL_KEY_SW_1_PXIFG = ~(HAL_KEY_SW_1_BIT);  /* Clear any pending interrupt */
        HAL_KEY_SW_2_ICTL |= HAL_KEY_SW_2_ICTLBIT; /* enable interrupt generation at port */
        HAL_KEY_SW_2_PXIFG = ~(HAL_KEY_SW_2_BIT);  /* Clear any pending interrupt */

    #else
        /* Rising/Falling edge configuratinn */
        PICTL &= ~(HAL_KEY_SW_6_EDGEBIT);    /* Clear the edge bit */
        /* For falling edge, the bit must be set. */
      #if (HAL_KEY_SW_6_EDGE == HAL_KEY_FALLING_EDGE)
        PICTL |= HAL_KEY_SW_6_EDGEBIT;
      #endif


        /* Interrupt configuration:
         * - Enable interrupt generation at the port
         * - Enable CPU interrupt
         * - Clear any pending interrupt
         */
        HAL_KEY_SW_6_ICTL |= HAL_KEY_SW_6_ICTLBIT;
        HAL_KEY_SW_6_IEN |= HAL_KEY_SW_6_IENBIT;
        HAL_KEY_SW_6_PXIFG = ~(HAL_KEY_SW_6_BIT);

        /* Rising/Falling edge configuratinn */
        HAL_KEY_JOY_MOVE_ICTL &= ~(HAL_KEY_JOY_MOVE_EDGEBIT);    /* Clear the edge bit */
        /* For falling edge, the bit must be set. */
      #if (HAL_KEY_JOY_MOVE_EDGE == HAL_KEY_FALLING_EDGE)
        HAL_KEY_JOY_MOVE_ICTL |= HAL_KEY_JOY_MOVE_EDGEBIT;
      #endif


        /* Interrupt configuration:
         * - Enable interrupt generation at the port
         * - Enable CPU interrupt
         * - Clear any pending interrupt
         */
        HAL_KEY_JOY_MOVE_ICTL |= HAL_KEY_JOY_MOVE_ICTLBIT;
        HAL_KEY_JOY_MOVE_IEN |= HAL_KEY_JOY_MOVE_IENBIT;
        HAL_KEY_JOY_MOVE_PXIFG = ~(HAL_KEY_JOY_MOVE_BIT);
    #endif // !CC2540_MINIDK

        /* Do this only after the hal_key is configured - to work with sleep stuff */
        if (HalKeyConfigured == TRUE)
        {
          osal_stop_timerEx(Hal_TaskID, HAL_KEY_EVENT);  /* Cancel polling if active */
        }
      }
      else    /* Interrupts NOT enabled */
      {
    #if defined ( CC2540_MINIDK )
        HAL_KEY_SW_1_ICTL &= ~(HAL_KEY_SW_1_ICTLBIT); /* don't generate interrupt */
        HAL_KEY_SW_2_ICTL &= ~(HAL_KEY_SW_2_ICTLBIT); /* don't generate interrupt */
    #else
        HAL_KEY_SW_6_ICTL &= ~(HAL_KEY_SW_6_ICTLBIT); /* don't generate interrupt */
        HAL_KEY_SW_6_IEN &= ~(HAL_KEY_SW_6_IENBIT);   /* Clear interrupt enable bit */
    #endif  // !CC2540_MINIDK

        osal_set_event(Hal_TaskID, HAL_KEY_EVENT);
      }

      /* Key now is configured */
      HalKeyConfigured = TRUE;
    }


    /**************************************************************************************************
     * @fn      HalKeyRead
     *
     * @brief   Read the current value of a key
     *
     * @param   None
     *
     * @return  keys - current keys status
     **************************************************************************************************/
    uint8 HalKeyRead ( void )
    {
      uint8 keys = 0;

    #if defined (CC2540_MINIDK)
      if (!(HAL_KEY_SW_1_PORT & HAL_KEY_SW_1_BIT))    /* Key is active low */
      {
        keys |= HAL_KEY_SW_1;
      }
      if (!(HAL_KEY_SW_2_PORT & HAL_KEY_SW_2_BIT))    /* Key is active low */
      {
        keys |= HAL_KEY_SW_2;
      }
    #else
    #ifdef HAL_BOARD_CC2530EB_REV17
      if ( (HAL_KEY_SW_6_PORT & HAL_KEY_SW_6_BIT))    /* Key is active high */
    #elif defined (HAL_BOARD_CC2530EB_REV13)
      if (!(HAL_KEY_SW_6_PORT & HAL_KEY_SW_6_BIT))    /* Key is active low */
    #endif
      {
        keys |= HAL_KEY_SW_6;
      }

      if ((HAL_KEY_JOY_MOVE_PORT & HAL_KEY_JOY_MOVE_BIT))  /* Key is active low */
      {
        keys |= halGetJoyKeyInput();
      }
    #endif
      return keys;
    }


    /**************************************************************************************************
     * @fn      HalKeyPoll
     *
     * @brief   Called by hal_driver to poll the keys
     *
     * @param   None
     *
     * @return  None
     **************************************************************************************************/
    void HalKeyPoll (void)
    {
      uint8 keys = 0;
      uint8 notify = 0;
    #if defined (CC2540_MINIDK)
      if (!(HAL_KEY_SW_1_PORT & HAL_KEY_SW_1_BIT))    /* Key is active low */
      {
        keys |= HAL_KEY_SW_1;
      }
      if (!(HAL_KEY_SW_2_PORT & HAL_KEY_SW_2_BIT))    /* Key is active low */
      {
        keys |= HAL_KEY_SW_2;
      }
    #else
      if (!(HAL_KEY_SW_6_PORT & HAL_KEY_SW_6_BIT))    /* Key is active low */
      {
        keys |= HAL_KEY_SW_6;
      }

      if ((HAL_KEY_JOY_MOVE_PORT & HAL_KEY_JOY_MOVE_BIT))  /* Key is active HIGH */
      {
        keys = halGetJoyKeyInput();
      }
    #endif

      /* If interrupts are not enabled, previous key status and current key status
       * are compared to find out if a key has changed status.
       */
      if (!Hal_KeyIntEnable)
      {
        if (keys == halKeySavedKeys)
        {
          /* Exit - since no keys have changed */
          return;
        }
        else
        {
          notify = 1;
        }
      }
      else
      {
        /* Key interrupt handled here */
        if (keys)
        {
          notify = 1;
        }
      }

      /* Store the current keys for comparation next time */
      halKeySavedKeys = keys;

      /* Invoke Callback if new keys were depressed */
      if (notify && (pHalKeyProcessFunction))
      {
        (pHalKeyProcessFunction) (keys, HAL_KEY_STATE_NORMAL);

      }
    }

    #if !defined ( CC2540_MINIDK )
    /**************************************************************************************************
     * @fn      halGetJoyKeyInput
     *
     * @brief   Map the ADC value to its corresponding key.
     *
     * @param   None
     *
     * @return  keys - current joy key status
     **************************************************************************************************/
    uint8 halGetJoyKeyInput(void)
    {
      /* The joystick control is encoded as an analog voltage.
       * Read the JOY_LEVEL analog value and map it to joy movement.
       */
      uint8 adc;
      uint8 ksave0 = 0;
      uint8 ksave1;

      /* Keep on reading the ADC until two consecutive key decisions are the same. */
      do
      {
        ksave1 = ksave0;    /* save previouse key reading */

        adc = HalAdcRead (HAL_KEY_JOY_CHN, HAL_ADC_RESOLUTION_8);

        if ((adc >= 2) && (adc <= 38))
        {
           ksave0 |= HAL_KEY_UP;
        }
        else if ((adc >= 74) && (adc <= 88))
        {
          ksave0 |= HAL_KEY_RIGHT;
        }
        else if ((adc >= 60) && (adc <= 73))
        {
          ksave0 |= HAL_KEY_LEFT;
        }
        else if ((adc >= 39) && (adc <= 59))
        {
          ksave0 |= HAL_KEY_DOWN;
        }
        else if ((adc >= 89) && (adc <= 100))
        {
          ksave0 |= HAL_KEY_CENTER;
        }
      } while (ksave0 != ksave1);

      return ksave0;
    }
    #endif

    /**************************************************************************************************
     * @fn      halProcessKeyInterrupt
     *
     * @brief   Checks to see if it's a valid key interrupt, saves interrupt driven key states for
     *          processing by HalKeyRead(), and debounces keys by scheduling HalKeyRead() 25ms later.
     *
     * @param
     *
     * @return
     **************************************************************************************************/
    void halProcessKeyInterrupt (void)
    {
      bool valid=FALSE;

    #if defined ( CC2540_MINIDK )
      if( HAL_KEY_SW_1_PXIFG & HAL_KEY_SW_1_BIT) /* Interrupt Flag has been set by SW1 */
      {
        HAL_KEY_SW_1_PXIFG = ~(HAL_KEY_SW_1_BIT); /* Clear Interrupt Flag */
        valid = TRUE;
      }

      if (HAL_KEY_SW_2_PXIFG & HAL_KEY_SW_2_BIT)  /* Interrupt Flag has been set by SW2 */
      {
        HAL_KEY_SW_2_PXIFG = ~(HAL_KEY_SW_2_BIT); /* Clear Interrupt Flag */
        valid = TRUE;
      }
    #else
      if (HAL_KEY_SW_6_PXIFG & HAL_KEY_SW_6_BIT)  /* Interrupt Flag has been set */
      {
        HAL_KEY_SW_6_PXIFG = ~(HAL_KEY_SW_6_BIT); /* Clear Interrupt Flag */
        valid = TRUE;
      }

      if (HAL_KEY_JOY_MOVE_PXIFG & HAL_KEY_JOY_MOVE_BIT)  /* Interrupt Flag has been set */
      {
        HAL_KEY_JOY_MOVE_PXIFG = ~(HAL_KEY_JOY_MOVE_BIT); /* Clear Interrupt Flag */
        valid = TRUE;
      }
    #endif
      if (valid)
      {
        osal_start_timerEx (Hal_TaskID, HAL_KEY_EVENT, HAL_KEY_DEBOUNCE_VALUE);
      }
    }

    /**************************************************************************************************
     * @fn      HalKeyEnterSleep
     *
     * @brief  - Get called to enter sleep mode
     *
     * @param
     *
     * @return
     **************************************************************************************************/
    void HalKeyEnterSleep ( void )
    {
    }

    /**************************************************************************************************
     * @fn      HalKeyExitSleep
     *
     * @brief   - Get called when sleep is over
     *
     * @param
     *
     * @return  - return saved keys
     **************************************************************************************************/
    uint8 HalKeyExitSleep ( void )
    {
      /* Wake up and read keys */
      return ( HalKeyRead () );
    }

    /***************************************************************************************************
     *                                    INTERRUPT SERVICE ROUTINE
     ***************************************************************************************************/

    /**************************************************************************************************
     * @fn      halKeyPort0Isr
     *
     * @brief   Port0 ISR
     *
     * @param
     *
     * @return
     **************************************************************************************************/
    HAL_ISR_FUNCTION( halKeyPort0Isr, P0INT_VECTOR )
    {
      HAL_ENTER_ISR();

    #if defined ( CC2540_MINIDK )
      if ((HAL_KEY_SW_1_PXIFG & HAL_KEY_SW_1_BIT) || (HAL_KEY_SW_2_PXIFG & HAL_KEY_SW_2_BIT))
    #else
      if (HAL_KEY_SW_6_PXIFG & HAL_KEY_SW_6_BIT)
    #endif
      {
        halProcessKeyInterrupt();
      }

      /*
        Clear the CPU interrupt flag for Port_0
        PxIFG has to be cleared before PxIF
      */
    #if defined ( CC2540_MINIDK )
      HAL_KEY_SW_1_PXIFG = 0;
      HAL_KEY_SW_2_PXIFG = 0;
    #else
      HAL_KEY_SW_6_PXIFG = 0;
    #endif
      HAL_KEY_CPU_PORT_0_IF = 0;

      CLEAR_SLEEP_MODE();

      HAL_EXIT_ISR();

      return;
    }

    #if !defined ( CC2540_MINIDK )
    /**************************************************************************************************
     * @fn      halKeyPort2Isr
     *
     * @brief   Port2 ISR
     *
     * @param
     *
     * @return
     **************************************************************************************************/
    HAL_ISR_FUNCTION( halKeyPort2Isr, P2INT_VECTOR )
    {
      HAL_ENTER_ISR();

      if (HAL_KEY_JOY_MOVE_PXIFG & HAL_KEY_JOY_MOVE_BIT)
      {
        halProcessKeyInterrupt();
      }

      /*
        Clear the CPU interrupt flag for Port_2
        PxIFG has to be cleared before PxIF
        Notes: P2_1 and P2_2 are debug lines.
      */
      HAL_KEY_JOY_MOVE_PXIFG = 0;
      HAL_KEY_CPU_PORT_2_IF = 0;

      CLEAR_SLEEP_MODE();

      HAL_EXIT_ISR();

      return;
    }
    #endif
    #else

    void HalKeyInit(void){}
    void HalKeyConfig(bool interruptEnable, halKeyCBack_t cback){}
    uint8 HalKeyRead(void){ return 0;}
    void HalKeyPoll(void){}

    #endif
    /**************************************************************************************************
    **************************************************************************************************/

    代码如何简化?

  • 这个写的很好了,我感觉不需要简化。如果只用一个按键,你可以去掉没用的按键的程序啊
  • 难度很大!

    按键不一样,中断也不一样的!

    有的函数封装成库函数没法修改。

    编程风格与原来传统的相差很远!