你好,首先谢谢你的回复。我想提的问题是,GATT_Notification(connHandle, ¬i, FALSE)这个函数怎么用?我怎么没找到这个函数的定义。比如我定义了一个数组 unsigned int Send[260] = {......};怎么把这个数组的数据全部发送到上位机上。蓝牙4.0一帧最多能发多少个数据啊???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,首先谢谢你的回复。我想提的问题是,GATT_Notification(connHandle, ¬i, FALSE)这个函数怎么用?我怎么没找到这个函数的定义。比如我定义了一个数组 unsigned int Send[260] = {......};怎么把这个数组的数据全部发送到上位机上。蓝牙4.0一帧最多能发多少个数据啊???
/*
* Send Data
*/
static void sendData(void )
{
static uint16 counter=0;
uint8 burstData[20] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
burstData[0] = (counter & 0xFF00)>>8;
burstData[1] = (counter & 0xFF);
attHandleValueNoti_t nData;
nData.len = 20;
nData.handle = 20;
//skKeyPressed = *((uint8*)pValue);
osal_memcpy( &nData.value, &burstData, 20 );
// Send the Notification
if (GATT_Notification( 0, &nData, FALSE )==SUCCESS)
{
counter++;
}
if(counter >1000)
{
osal_stop_timerEx(simpleBLEPeripheral_TaskID,SBP_BURST_EVT);
counter = 0;
}
}
应用参考如上,260个字节的发送需要分包。每包20个字节。你可以在论坛搜索一下GATT_Notification .
分包发送如下,这里 #define SBP_BURST_EVT_PERIOD 7
if ( events & SBP_BURST_EVT )
{
// Restart timer
if ( SBP_BURST_EVT_PERIOD )
{
osal_start_timerEx( simpleBLEPeripheral_TaskID, SBP_BURST_EVT, SBP_BURST_EVT_PERIOD );
}
sendData();
sendData();
sendData();
sendData();
//burstData[0] = !burstData[0];
return (events ^ SBP_BURST_EVT);
}