This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC2652RB: 发送周期广播数据失败

Part Number: LP-CC2652RB

我按照SimpleLinkTm CC13x2 / CC26x2 SDK BLE5-Stack User's Guide 2.02.01.00中周期广播那节的指导步骤进行外设设备的代码编写,

但主机centor设备无法接收到通过GapAdv_SetPeriodicAdvData函数设置的周期广播数据,但可以接收到GapAdv_loadByHandle设置的数据。附上外设设备配置周期广播部分的代码段如下,各函数返回的status我已经检查过,都返回了SUCCESS

// Periodic Advertising Intervals
#define PERIDIC_ADV_INTERVAL_MIN    160  
#define PERIDIC_ADV_INTERVAL_MAX    160 

/// Non-Connectable & Non-Scannable advertising set
#define GAPADV_PARAMS_AE_NC_NS {                                           \
  .eventProps = 0,                                                         \
  .primIntMin = 160,                                                       \
  .primIntMax = 160,                                                       \
  .primChanMap = GAP_ADV_CHAN_ALL,                                         \
  .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID,                       \
  .peerAddr = { 0x74, 0xD2, 0x85, 0xD4, 0x63, 0xB4 },                      \
  .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ,                               \
  .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE,                               \
  .primPhy = GAP_ADV_PRIM_PHY_1_MBPS,                                      \
  .secPhy = GAP_ADV_SEC_PHY_1_MBPS,                                        \
  .sid = 1                                                                \
}

static uint8 advHandleNCNS;      // Non-Connactable & Non-Scannable

static uint8_t periodicData[] =
{
  'P',
  'e',
  'r',
  'i',
  'o',
  'd',
  'i',
  'c',
  'A',
  'd',
  'v'
};

#define GAPADV_DATA_PERIODIC_ADV {                          \
   .operation = GAPADV_PERIODIC_ADV_DATA_COMPLETE,           \
   .dataLength = sizeof(periodicData),                       \
   .pData = periodicData                                     \
 }

// Advertisement data
static uint8_t advertData[] =
{
  0x0C,                         // Length of this data
  GAP_ADTYPE_LOCAL_NAME_SHORT,  // Type of this data
  'P',
  'e',
  'r',
  'i',
  'o',
  'd',
  'i',
  'c',
  'A',
  'd',
  'v',
  0x02,   // length of this data
  GAP_ADTYPE_FLAGS,
  GAP_ADTYPE_FLAGS_GENERAL | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,
};

// Create non connectable & non scannable advertising set #3
GapAdv_params_t advParamNonConn = GAPADV_PARAMS_AE_NC_NS;

// Create Advertisement set #3 and assign handle
status = GapAdv_create(&SimplePeripheral_advCallback, &advParamNonConn, &advHandleNCNS);

// Load advertising data for set #3 that is statically allocated by the app
status = GapAdv_loadByHandle(advHandleNCNS, GAP_ADV_DATA_TYPE_ADV,
                             sizeof(advertData), advertData);

// Set event mask for set #3
status = GapAdv_setEventMask(advHandleNCNS,
                             GAP_ADV_EVT_MASK_START_AFTER_ENABLE |
                             GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
                             GAP_ADV_EVT_MASK_SET_TERMINATED);

// Enable non connectable & non scannable advertising for set #3
status = GapAdv_enable(advHandleNCNS, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);

// Set Periodic Advertising parameters
GapAdv_periodicAdvParams_t perParams = {PERIDIC_ADV_INTERVAL_MIN,
                                        PERIDIC_ADV_INTERVAL_MAX, 0x40};
status = GapAdv_SetPeriodicAdvParams(advHandleNCNS, &perParams);

GapAdv_periodicAdvData_t periodicDataParams = GAPADV_DATA_PERIODIC_ADV;
status = GapAdv_SetPeriodicAdvData(advHandleNCNS, &periodicDataParams);

// Enable the periodic advertising
status = GapAdv_SetPeriodicAdvEnable(1, advHandleNCNS);

经过在论坛搜索,我找到了之前的一个帖子[参考译文] LAUNCHXL-CC26X2R1:BTool 中发送周期性广播包的正确方法是什么? - Bluetooth®︎(参考译文帖)(Read Only) - Bluetooth®︎(参考译文帖) - E2ETm 设计支持 (ti.com),问题描述与我目前的现象基本一样,目前我仍没有找到问题原因和解决方法。

  • 您好,

    我们需要一点时间查看这个问题,有结论后及时联系您。

  • 好的,感谢!

  • 您好,

    这个问题我们帮您升级到E2E英文论坛由专业产线工程师帮您解答,有回复及时联系您。

    这边希望您提供一下相关正在使用的SDK版本

  • 您好,目前正在使用的SDK版本为simplelink_cc13x2_26x2_sdk_5_10_00_48

  • 您好,

    您必须在 simple_central 进行一些额外的代码修改才能捕获周期性广告。这些修改写在了 Synchronize with a Periodic Advertising Train 部分中。您是否实施了这些步骤?

  • 抱歉,上周没有及时回复您。

    附上我的simple_central代码

    初始化相关代码如下:

    void SimpleCentral_scanCb(uint32_t evt, void* pMsg, uintptr_t arg)
    {
      uint8_t event;
    
      if (evt & GAP_EVT_ADV_REPORT)
      {
        event = SC_EVT_ADV_REPORT;
      }
      else if (evt & GAP_EVT_SCAN_ENABLED)
      {
        event = SC_EVT_SCAN_ENABLED;
      }
      else if (evt & GAP_EVT_SCAN_DISABLED)
      {
        event = SC_EVT_SCAN_DISABLED;
      }
      else if (evt & GAP_EVT_INSUFFICIENT_MEMORY)
      {
        event = SC_EVT_INSUFFICIENT_MEM;
      }
      else
      {
        return;
      }
    
      if(SimpleCentral_enqueueMsg(event, SUCCESS, pMsg) != SUCCESS)
      {
        ICall_free(pMsg);
      }
    }
    
    GapScan_registerCb(SimpleCentral_scanCb, NULL);
    
    // Set Scanner Event Mask
    GapScan_setEventMask(GAP_EVT_SCAN_ENABLED | GAP_EVT_SCAN_DISABLED |
                       GAP_EVT_ADV_REPORT);
    
    // Set Scan PHY parameters
    GapScan_setPhyParams(DEFAULT_SCAN_PHY, SCAN_TYPE_PASSIVE,
                       DEFAULT_SCAN_INTERVAL, DEFAULT_SCAN_WINDOW);
    
    // Set Advertising report fields to keep
    temp16 = (SCAN_ADVRPT_FLD_ADDRESS | SCAN_ADVRPT_FLD_ADDRTYPE);
    GapScan_setParam(SCAN_PARAM_RPT_FIELDS, &temp16);
    // Set Scanning Primary PHY
    temp8 = SCAN_PRIM_PHY_1M;
    GapScan_setParam(SCAN_PARAM_PRIM_PHYS, &temp8);
    // Set LL Duplicate Filter
    temp8 = SCAN_FLT_DUP_ENABLE;
    GapScan_setParam(SCAN_PARAM_FLT_DUP, &temp8);
    
    temp16 = SCAN_FLT_PDU_NONCONNECTABLE_ONLY;
    GapScan_setParam(SCAN_PARAM_FLT_PDU_TYPE, &temp16);
    
    // Set initiating PHY parameters
    // INIT_PHYPARAM_MAX_CONN_INT = 80
    GapInit_setPhyParam(INIT_PHY_1M, INIT_PHYPARAM_CONN_INT_MIN,
    				  INIT_PHYPARAM_MIN_CONN_INT);
    GapInit_setPhyParam(INIT_PHY_1M, INIT_PHYPARAM_CONN_INT_MAX,
    				  INIT_PHYPARAM_MAX_CONN_INT);

    在SimpleCentral_processAppMsg函数中关于SC_EVT_ADV_REPORT广播扫描报告事件的处理中,我加了打印,第一个现象是没看到pAdvRpt->periodicAdvInt != 0的周期广播数据,第二个现象是发现了我的simple_peripheral设置的GapAdv_loadByHandle广播数据,代码如下:

    static void SimpleCentral_processAppMsg(scEvt_t *pMsg)
    {
      bool safeToDealloc = TRUE;
    
      if (pMsg->hdr.event <= APP_EVT_EVENT_MAX)
      {
        BLE_LOG_INT_STR(0, BLE_LOG_MODULE_APP, "APP : App msg status=%d, event=%s\n", 0, appEventStrings[pMsg->hdr.event]);
      }
      else
      {
        BLE_LOG_INT_INT(0, BLE_LOG_MODULE_APP, "APP : App msg status=%d, event=0x%x\n", 0, pMsg->hdr.event);
      }
    
      switch (pMsg->hdr.event)
      {
        case SC_EVT_KEY_CHANGE:
          SimpleCentral_handleKeys(pMsg->hdr.state);
          break;
    
        case SC_EVT_ADV_REPORT:
        {
          GapScan_Evt_AdvRpt_t* pAdvRpt = (GapScan_Evt_AdvRpt_t*) (pMsg->pData);
            if(0 != pAdvRpt->periodicAdvInt)
            {
             // this is a periodic advertisement
                Display_printf(dispHandle, SC_ROW_9, 0, "this is a periodic advertisement");
                SimpleCentral_doStopDiscovering(0);
            }
            else
            {
             // this is NOT a periodic advertisement
            }
            // reporting the advData according to the peripheral address
            if(pAdvRpt->addr[0] == 0x8c && pAdvRpt->addr[5] == 0x74) { // this is my peripheral address
                Display_printf(dispHandle, SC_ROW_NON_CONN, 0, "Discovered: %s", Util_convertBdAddr2Str(pAdvRpt->addr));
                int j = 0;
                Display_printf(dispHandle, SC_ROW_9 + 1, 0, "advertisement data len: %d", pAdvRpt->dataLen);
                for(j = 0; j < pAdvRpt->dataLen; j++) {
                    Display_printf(dispHandle, SC_ROW_9 + 2 + j, 0, "%x", *(pAdvRpt->pData + j));
                }
            }
          
    
          // Free report payload data
          if (pAdvRpt->pData != NULL)
          {
            ICall_free(pAdvRpt->pData);
          }
          break;
        }
        
        // ...
        
        default:
          // Do nothing.
          break;
    }

    根据 Synchronize with a Periodic Advertising Train中的步骤来看,目前我在第六步遇到了问题,无法识别到periodic advertisers

  • 您好,

    我建议您首先验证 advertiser 是否实际发送定期广告。这可以通过使用逻辑分析仪和使用RF调试引脚来完成,您可以像这样启用。

    https://dev.ti.com/tirex/content/simplelink_cc13xx_cc26xx_sdk_6_41_00_17/docs/ble5stack/ble_user_guide/html/ble-stack-5.x-guide/debugging-index.html#debugging-rf-output

    我还建议您使用GAPADV_PERIODIC_ADV_ENABLE_TX_POWER而不是使用0x40 hex value。

    一旦您确认 advertiser 实际上正在发送定期广告,就可以看到如何让 central 可以同步到他们。