怎么将P1口设为外部中断呢?就像P0口的按键一样使用,试了几天了还是不行。
求TI的工程师和路过的各位大神能指点一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好的,下面就是我改动的程序:
/* CPU port interrupt */
#define HAL_KEY_CPU_PORT_0_IF P0IF
#define HAL_KEY_CPU_PORT_1_IF P2IF
#define HAL_KEY_CPU_PORT_2_IF P2IF
#if defined ( CC2540_MINIDK )||( WEBEE_BOARD )
/* SW_1 is at P0.0 */
#define HAL_KEY_SW_1_PORT P0
#define HAL_KEY_SW_1_BIT BV(0)
#define HAL_KEY_SW_1_SEL P0SEL
#define HAL_KEY_SW_1_DIR P0DIR
/* SW_2 is at P1.6 */
#define HAL_KEY_SW_2_PORT P1
#define HAL_KEY_SW_2_BIT BV(6)
#define HAL_KEY_SW_2_SEL P1SEL
#define HAL_KEY_SW_2_DIR P1DIR
#define HAL_KEY_SW_1_IEN IEN1 /* CPU interrupt mask register */
#define HAL_KEY_SW_1_ICTL P0IEN /* Port Interrupt Control register */
#define HAL_KEY_SW_1_ICTLBIT BV(0) /* P0IEN - P0.0 enable/disable bit */
#define HAL_KEY_SW_1_IENBIT BV(5) /* Mask bit for all of Port_0 */
#define HAL_KEY_SW_1_PXIFG P0IFG /* Interrupt flag at source */
#define HAL_KEY_SW_2_IEN IEN2 /* CPU interrupt mask register */
#define HAL_KEY_SW_2_ICTL P1IEN /* Port Interrupt Control register */
#define HAL_KEY_SW_2_ICTLBIT BV(6) /* P0IEN - P0.1 enable/disable bit */
#define HAL_KEY_SW_2_IENBIT BV(4) /* Mask bit for all of Port_0 */
#define HAL_KEY_SW_2_PXIFG P1IFG /* Interrupt flag at source */
#define HAL_KEY_SW_1_EDGEBIT BV(0)
#else
//P0口中断程序
HAL_ISR_FUNCTION( halKeyPort0Isr, P0INT_VECTOR )
{
HAL_ENTER_ISR();
#if defined ( CC2540_MINIDK )||( WEBEE_BOARD )
if ((HAL_KEY_SW_1_PXIFG & HAL_KEY_SW_1_BIT))
#else
if (HAL_KEY_SW_6_PXIFG & HAL_KEY_SW_6_BIT)
#endif
{
halProcessKeyInterrupt();
}
#if defined ( CC2540_MINIDK )||( WEBEE_BOARD )
HAL_KEY_SW_1_PXIFG = 0;
HAL_KEY_SW_2_PXIFG = 0;
#else
HAL_KEY_SW_6_PXIFG = 0;
#endif
HAL_KEY_CPU_PORT_0_IF = 0;
CLEAR_SLEEP_MODE();
HAL_EXIT_ISR();
return;
}
//P1口中断程序
HAL_ISR_FUNCTION( halKeyPort1Isr, P1INT_VECTOR )
{
HAL_ENTER_ISR();
#if defined ( CC2540_MINIDK )||( WEBEE_BOARD )
if ((HAL_KEY_SW_2_PXIFG & HAL_KEY_SW_2_BIT))
#else
if (HAL_KEY_SW_6_PXIFG & HAL_KEY_SW_6_BIT)
#endif
{
halProcessKeyInterrupt();
}
#if defined ( CC2540_MINIDK )||( WEBEE_BOARD )
HAL_KEY_SW_1_PXIFG = 0;
HAL_KEY_SW_2_PXIFG = 0;
#else
HAL_KEY_SW_6_PXIFG = 0;
#endif
HAL_KEY_CPU_PORT_1_IF = 0;
CLEAR_SLEEP_MODE();
HAL_EXIT_ISR();
return;
}
//下面的是初始化部分
P0SEL = 0; // Configure Port 0 as GPIO
P1SEL = 0; // Configure Port 1 as GPIO
P2SEL = 0; // Configure Port 2 as GPIO
P0DIR = 0xFC;
P1DIR = 0xBF;
P2DIR = 0x1F;
P0 = 0x03;
P1 = 0x40;
P2 = 0;
// 这里是按键的函数
#if defined( CC2540_MINIDK )||( WEBEE_BOARD )
int num;
static void simpleBLEPeripheral_HandleKeys( uint8 shift, uint8 keys )
{
VOID shift; // Intentionally unreferenced parameter
if (keys & HAL_KEY_SW_1)
{
num--;
}
if(keys & HAL_KEY_SW_2)
{
num++;
}
}
#endif
所有改动的部分都在这里了,麻烦您帮忙看看问题究竟在哪?我看了好多次了还是不行,谢谢了
在cc2540 usb dongle 测试通过!
中断功能:按键闪灯!
#include "ioCC2540.h"
void delay(void)
{unsigned long i;
for(i=0;i<100000;i++)
asm(" nop ");
}
#pragma vector = P1INT_VECTOR
__interrupt void P1INT_ISR(void)
{P1IFG=0;
P1IF=0;
P0=0;
delay();
delay();
delay();
P0=0xff;
delay();
delay();
delay();
}
void main()
{
P0SEL =0;
P1SEL =0x0;
P0DIR=0xff;
P1DIR=0x02;
PICTL = 0x02;
P1IEN=0x0c;
IEN2=0x10;
EA=1;
while(1)
{
}
}
谢谢了,大秦正声,在单片机上运行的程序我也做过,并且可以使用,但是在协议栈上就不行了,不知道是怎么回事,可以在帮忙看看吗?
http://www.deyisupport.com/question_answer/wireless_connectivity/bluetooth/f/103/p/68255/161765.aspx#161765 请看我原来回答的帖子,帖子是将P0的按键换成P1的。
另外老外的函数看起来拐弯很多,但是读懂之后,修改就很通用,只需改挤出宏定义即可。逻辑性很强