This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【CC2541】interrupt不触发问题



Hi engineers,

目前我们系统使用kionix kxcj9-1008加速度传感器,使用interrupt方式接收处理数据,在工作一段时间后发现interrupt再也无法触发,由于kionix加速度传感器需要release一个register才能再被触发,因此我是在interrupt读取数据后去release kionix加速度传感器使它能再次触发中断。

请问,在什么情况下会使interrupt不触发,或者需要怎样能保证interrupt一定能触发,需要加critical section吗?

我在interrupt里面代码如下,请帮忙review一下是否需要修改?

HAL_ISR_FUNCTION( halAccelPort1Isr, P1INT_VECTOR )
{
HAL_ENTER_ISR();
/* Make sure we're processing the desired interrupt */
if ((P1IFG & HAL_ACCEL_P1_INTERRUPT_PINS) && (P1IEN & HAL_ACCEL_P1_INTERRUPT_PINS))
{
   xxx_triger_acc_interrupt_read();//该函数中会release kionix中断,使能再次触发interrupt
}

P1IFG = 0;
P1IF = 0;
HAL_EXIT_ISR();
}