This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于PM3的进入和退出问题的提问?

Other Parts Discussed in Thread: CC2540, CC2544

请问一下,如何可以让系统进入PM3工作模式?在PM3工作模式下,只有复位和外部中断可以唤醒,那么如何在外部中断中加入函数,才可以唤醒呢?两个问题,有没有大神解释一下。先谢谢了!

  • 只要没有其他定时事件,协议栈可以进入PM3。可以参考STACK中Advremote例子,这就是个遥控器,没有连接时进入PM3靠按键激活

    可以参考帖子 http://www.deyisupport.com/question_answer/wireless_connectivity/bluetooth/f/103/t/25190.aspx

  • 协议栈中已经写好了休眠函数,在没有定时时间时自动进入(因为PM3时定时器不工作,所以定时事件下是无法进入PM3的)。 PM3就是靠外部中断唤醒的,可以是按键、或者光敏三极管的外部中断,都可以退出,SImplePeripheral工程中对按键的中断程序已经写好,您可以参考

  • 可以参考下边的例程!可以移植到cc2540!

    /***********************************************************************************
      Filename:     powermode3.c

      Description:  This software example shows how to properly enter Power Mode 3
                    and then exit upon Port 0 Interrupt. The SRF05EB LED1 is cleared
                    before entering Power Mode 3, and then set by the Port 0 ISR.
                    Hence, the LED1 is ON in Active Mode and OFF in Power Mode 3.

      Note:         PM2 and PM3 is not supported on the CC2544.

    ***********************************************************************************/

    /***********************************************************************************
    * INCLUDES
    */
    #include <power_mode.h>
    #include <hal_types.h>
    // Include Name definitions of individual bits and bit-fields in the CC254x device registers.
    #include <ioCC254x_bitdef.h>
    // Include device specific file
    #if (chip==2541)
    #include "ioCC2541.h"
    #elif (chip==2543)
    #include "ioCC2543.h"
    #elif (chip==2545)
    #include "ioCC2545.h"
    #else
    #error "Chip not supported!"
    #endif


    /***********************************************************************************
    * CONSTANTS
    */
    // Wait time in Active mode.
    #define ACT_MODE_TIME  50000


    /***********************************************************************************
    * LOCAL VARIABLES
    */
    // Variable for active mode duration.
    static uint32 __xdata activeModeCnt = 0;


    /***********************************************************************************
    * LOCAL FUNCTIONS
    */

    /***********************************************************************************
    * @fn          setup_port_interrupt
    *
    * @brief       Function which sets up the Port 0 Interrupt for Power Mode 3 usage.
    *
    * @param       void
    *
    * @return      void
    */
    void setup_port_interrupt(void)
    {
        // Clear Port 0 Interrupt flags.
        P0IF = 0;
        P0IFG = 0x00;

        // Interrupt enable on all pins on port 0.
        P0IEN = 0xFF;  

        // Enable CPU Interrupt for Port 0 (IEN1.P0IE = 1).
        P0IE = 1;

        // Enable Global Interrupt by setting the (IEN0.EA = 1).
        EA = 1;
    }


    /***********************************************************************************
    * @fn          port0_isr
    *
    * @brief       Port 0 Interrupt Service Routine, which executes when SRF05EB S1
    *              (P0_1) is pressed.
    *
    * @param       void
    *
    * @return      void
    */
    #pragma vector = P0INT_VECTOR
    __interrupt void port0_isr(void)
    {
        // Note that the order in which the following flags are cleared is important.

        // Clear Port 0 Interrupt Flags.
        P0IFG = 0x00;

        // Clear CPU Interrupt Flag for P0 (IRCON.P0IF = 0).
        P0IF = 0;

        // Set LED1 to indicate Active Mode.
        P1_0 = 1;
    }


    /***********************************************************************************
    * @fn          main
    *
    * @brief       Enter Power Mode, exit Power Mode 3 using Port 0 Interrupt.
    *
    * @param       none
    *
    * @return      0
    */

    void main(void)
    {
        /***************************************************************************
         * Setup I/O
         */
        // Initialize P1_0 for SRF05EB LED1.
        P1SEL &= ~BIT0;           // Function as General Purpose I/O.
        P1_0 = 1;                 // LED1 on.
        P1DIR |= BIT0;            // Output.

        // Initialize P0_1 for SRF05EB S1 button.
        P0SEL &= ~BIT1;           // Function as General Purpose I/O.
        P0DIR &= ~BIT1;           // Input.
        P0INP |= BIT1;            // 3-state input.


        /***************************************************************************
         * Setup interrupt
         *
         * Setup and enable Port 0 Interrupt, which shall wake-up the SoC from
         * Power Mode 3.
         */
        setup_port_interrupt();
       
       
        /***********************************************************************
         * Setup powermode
         */
        // Set [SLEEPCMD.MODE] to PM3.
        SLEEPCMD = (SLEEPCMD & ~SLEEPCMD_MODE) | SLEEPCMD_MODE_PM3;


        /* Main Loop, enter/exit Power Mode 3. */
        while(1)
        {
            // Wait some time in Active Mode, and clear LED1 before
            // entering Power Mode 3.
            for(activeModeCnt = 0; activeModeCnt < ACT_MODE_TIME; activeModeCnt++);
            P1_0 = 0;
           
            // Enter powermode
            // Sets PCON.IDLE with a 2-byte boundary assembly instruction.
            // NOTE: Cache must be enabled (see CM in FCTL).
            // This method gives the least current consumption.
            EnterSleepModeProcessInterruptsOnWakeup();
           
        }
    }


    /***********************************************************************************
      Copyright 2012 Texas Instruments Incorporated. All rights reserved.

      IMPORTANT: Your use of this Software is limited to those specific rights
      granted under the terms of a software license agreement between the user
      who downloaded the software, his/her employer (which must be your employer)
      and Texas Instruments Incorporated (the "License").  You may not use this
      Software unless you agree to abide by the terms of the License. The License
      limits your use, and you acknowledge, that the Software may not be modified,
      copied or distributed unless embedded on a Texas Instruments microcontroller
      or used solely and exclusively in conjunction with a Texas Instruments radio
      frequency transceiver, which is integrated into your product.  Other than for
      the foregoing purpose, you may not use, reproduce, copy, prepare derivative
      works of, modify, distribute, perform, display or sell this Software and/or
      its documentation for any purpose.

      YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
      PROVIDED 揂S IS?WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
      INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
      NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
      TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
      NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
      LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
      INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
      OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
      OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
      (INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.

      Should you have any questions regarding your right to use this Software,
      contact Texas Instruments Incorporated at www.TI.com.
    ***********************************************************************************/