This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

蓝牙发起连接请求到提示配对,这两个行为的间隔可不可以扩到到5S。



同上!

谢谢!

  • wenshuai,

    传统蓝牙还是BLE?

    这个是由任意一方决定的,而且是link layer底层的工作,一般没法控制。

  • 好的,谢谢!

  • Hi,Yan!

    我想问一下:蓝牙:BLE,实现目的:利用SIMPLEPROFILE_CHARX来实现最大数据量为0.5K的数据传输,且传输数据时,需要知道。  SIMPLEPROFILE_CHARX的读写和长度以及添加已经实现。

    目前思路:1.1数据传输:在两个BLE连接的状态下,  要传数据为char win[20],调用SimpleProfile_SetParameter( SIMPLEPROFILE_CHAR1,SIMPLEPROFILE_CHAR1_LEN,win );

    每个包最大20字节。调用SimpleProfile_SetParameter是因为论坛上说,连接时属性改变时,可以自动传输。(已实现)

                    1. 2.传输成功与否的验证调用完SimpleProfile_SetParameter后,如何知道发送成功或者失败。(暂未找到突破口,请指点!

                    2.我的这种思路是否可行,是否有更好的解决办法

                    3.传统的蓝牙传输歌曲什么,调用的是何种接口,BLE中是否有此类接口

                    谢谢!