This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2540密码问题



我想把配对密码读取出来,可是读出来一直是错误的,请帮我看下:

  // Setup the GAP Bond Manager
  {
    uint32 passkey = 0; // passkey "000000"
    uint8 pairMode = GAPBOND_PAIRING_MODE_INITIATE;
    uint8 mitm = TRUE;
    uint8 ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
    uint8 bonding = TRUE;
    GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof ( uint32 ), &passkey );
    GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof ( uint8 ), &pairMode );
    GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof ( uint8 ), &mitm );
    GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof ( uint8 ), &ioCap );
    GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof ( uint8 ), &bonding );
  }

static void ProcessPasscodeCB(uint8 *deviceAddr,uint16 connectionHandle,uint8 uiInputs,uint8 uiOutputs )
{

   uint32  passcode = 4444;


  // Send passcode response
  GAPBondMgr_PasscodeRsp( 0, SUCCESS, passcode );
}

 以下是读取:

 uint32 passcode;
  uint8   str[7];
  GAPRole_GetParameter(GAPBOND_DEFAULT_PASSCODE,&passcode);  
  SerialPrintString("passcode:");
  SerialPrintString( (unsigned char *) _ltoa(passcode, str, 10));

 

读出来的是:12063422,我在 ProcessPasscodeCB()改变值也没反应