This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于power_saving后无法连接的问题

Other Parts Discussed in Thread: CC2541

dear all:

   cc2541广播能够用手机上的lightblue检测到,但尝试去连接的时候就disconnect了,用usb dongle连接也是如此,信息如下:

23:23:25.385 > BLE Host: COM7 57600 baud hardware flowc.

23:23:25.786 > BLE Host found

23:23:25.789 > Scan request ...

23:23:25.789 > GAP Device Init Done

23:23:26.312 > GAP Device Information: 00 00 [len=7]

23:23:26.314 > MAC address: B4:99:4C:62:61:F8

23:23:26.332 > GAP Device Information: 00 04 [len=30]

23:23:26.332 > Device found: SimpleBLEPeripheral

23:23:26.333 > Scan resp: ad=0x12 len=5

23:23:26.333 > Scan resp: ad=0x0a len=2

23:23:29.838 > Scan cancel request ...

23:23:29.857 > Scan finished [4.68 sec]

23:23:29.858 > GAP Device Discovery: 0 devices

23:23:36.891 > Connect request

23:23:37.386 > Gap Link Established: h=0000 ci=25 lat=0 to=200

23:23:37.386 > SimpleBLEPeripheral connected

23:23:37.390 > Service discovery started

23:23:37.715 > ATT_ReadByGrpTypeRsp - status=0 n=19

23:23:37.805 > ATT_ReadByGrpTypeRsp - status=0 n=7

23:23:37.810 > ATT_ReadByGrpTypeRsp - status=26 n=0

23:23:37.810 > Primary Service Discovery done [0.422 sec]

23:23:37.827 > Characteristic description discovery started

23:23:37.872 > ATT_FindInfoRsp - status=0 n=21

23:23:39.867 > ATT_FindInfoRsp - status=20 n=0

23:23:39.873 > GAP Link Terminated: status=0 h=0 reason=0x08

23:23:39.874 > SimpleBLEPeripheral disconnected

然后如上情况只出现在电池供电,且power_saving的时候会出现。

当做如下操作的时候会消失:

1 用ccdebugger供电时,就是ok的(这里应该只有ccdebugger的电压高点这个区别吧?)

2 将power_saving中进入低功耗的设置:PM2,PM3都改为PM1时,问题消失。(PM1和PM2,3的区别是voltage regulator 的关闭与否,前者不关闭)


尝试:

1 本来怀疑32K的外接不行,进入低功耗后就挂了。尝试改为内部32K,问题依旧。(此时只进入pm2,没进入pm3)

2 同套模块在网上购买的成品模块上跑没有问题


望各位大神不吝赐教,给个反向也行