目前我用开发板上的主从一体程序,是可行的,但是增加HAL_UART=TRUE后,显示程序溢出。
求TI原版主从一体程序。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Yan:
我下载了这个例子,编译没有错误,但是增加了HAL_UART=TRUE之后,扔然提示溢出错误。
Error[e104]: Failed to fit all segments into specified ranges. Problem discovered in segment XDATA_N. Unable to place 2 block(s) (0xaf2 byte(s) total) in 0x9b9 byte(s) of memory. The problem occurred while processing the segment placement command "-P(XDATA)XDATA_N=_XDATA_START-_XDATA_END", where at the moment of placement the available memory ranges were "XDATA:1547-1eff"
这个错误和我原来使用的文件编译产生的错误一样,但是我的xcl文件也是采用的原始文件,并没有更改过,请问应该如何解决?
以下是我采用的定义:
INT_HEAP_LEN=2800
HALNODEBUG
OSAL_CBTIMER_NUM_TASKS=1
HAL_AES_DMA=TRUE
HAL_DMA=TRUE
POWER_SAVING
xPLUS_BROADCASTER
HAL_LCD=FALSE
HAL_LED=TRUE
CC2540_MINIDK
CC2541
HAL_UART=TRUE