和BTOOL连接后,连接不稳定,会断开。断开后有的时候BTOOL可以重新扫描到设备,有时候扫描不到。这是什么原因,该怎么办呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该不是,板子没动,之前没有出现过这样的问题啊
情况是这样:
1.一直能进入中断的时候,蓝牙方面就会有问题,有的时候是扫描不到从机,有的时候是连接上了自动断开。
2.刚开始能进入中断,之后就进不去了,我没有屏蔽中断。但是这时候是可以连接到btool的。
我的程序没有改动,下载进板子以后就会出现这两种情况,这会不会和程序进入中断太频繁,或者是执行了周期任务任务有关啊。程序里面开了两个中断,而且两个串口都一直有数据,也就是说程序应该是在不断的进入中断。中断里面只是接收数据,没有进行太多操作。程序里面还设置了两个周期任务,一个是200ms,一个是1s