This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: CC2340R5 评估问题

Part Number: LP-EM-CC2340R5

Hi,TI工程师您们好:

    目前有个应用想基于CC2340基础上进行开发设计,不过目前有些问题点想进一步确认。麻烦帮忙确认以下几个问题,谢谢

(1)cc2340支持设置TX Power的挡位值有哪些?可以设置哪些参数值

(2)Output power up to +8 dBm with temperature compensation?这个温度补偿是什么机制?是根据芯片温度来进行降低,如高温时,不是一定为8dbm?

(3)芯片内置温度传感器精度是多少?

  • 您好,

    芯片内置温度传感器精度是多少?

    您可以查看datasheet第8.8章节:

    Output power up to +8 dBm with temperature compensation?这个温度补偿是什么机制?是根据芯片温度来进行降低,如高温时,不是一定为8dbm?

    输出功率在整个温度范围内相对平坦,这是在不同温度下通过各种功率设置自动进行内部补偿的。

    cc2340支持设置TX Power的挡位值有哪些?可以设置哪些参数值

    现在的SDK暂时无法通过HCI 命令修改TX POWER,需要等待后续更新。

    感谢您的支持。