This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541接NTC测温,求教ADC

Other Parts Discussed in Thread: CC2541, OPA4379

NTC规格书上的最高和最低温度参数如下:

32.0℃  R=36.871kΩ,

42.0℃  R=24.448kΩ,

要求在这个温度范围内最大误差±0.2℃,其中36.0℃~39.0℃之间允许的误差为±0.1,直接用CC2541的ADC能做到么?

CC2541的ADC有8个输入通道,差分输入的话该接到哪个脚呢?

CR2302电池供电

请各位前辈、大神指点,多谢!