This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IOS 怎么获取外设的广播数据AdvData

Other Parts Discussed in Thread: CC2540

(void)centralManager:(CBCentralManager *)central didDiscoverPeripheral:(CBPeripheral *)peripheral advertisementData:(NSDictionary *)advertisementData RSSI:(NSNumber *)RSSI{ ……}

这个方法中的advertisementData只能抓取到下面的键值

{

    kCBAdvDataIsConnectable = 1;

    kCBAdvDataLocalName = SimpleBLEPeripheral;

    kCBAdvDataServiceUUIDs =     (        FFF0    );

    kCBAdvDataTxPowerLevel = 0;

}

simpleBLEPeripheral.c avertData数组的内容,也就是下图报文中的AdvData

  • Enjoy it ^_^ :

    NSArray *keys = [advertisementData allKeys];
        NSData *dataAmb, *dataObj;
        for (int i = 0; i < [keys count]; ++i) {
            id key = [keys objectAtIndex: i];
            NSString *keyName = (NSString *) key;
            NSObject *value = [advertisementData objectForKey: key];
            if ([value isKindOfClass: [NSArray class]]) {
                printf("   key: %s\n", [keyName cStringUsingEncoding: NSUTF8StringEncoding]);
                NSArray *values = (NSArray *) value;
                for (int j = 0; j < [values count]; ++j) {
                    if ([[values objectAtIndex: j] isKindOfClass: [CBUUID class]]) {
                        CBUUID *uuid = [values objectAtIndex: j];
                        NSData *data = uuid.data;
                        if (j == 0) {
                            dataObj = uuid.data;
                        } else {
                            dataAmb = uuid.data;
                        }
                        printf("      uuid(%d):", j);
                        for (int j = 0; j < data.length; ++j)
                            printf(" %02X", ((UInt8 *) data.bytes)[j]);
                        printf("\n");
                    } else {
                        const char *valueString = [[value description] cStringUsingEncoding: NSUTF8StringEncoding];
                        printf("      value(%d): %s\n", j, valueString);
                    }
                }
            } else {
                const char *valueString = [[value description] cStringUsingEncoding: NSUTF8StringEncoding];
                printf("   key: %s, value: %s\n", [keyName cStringUsingEncoding: NSUTF8StringEncoding], valueString);
            }
        }

  • 谢谢,可是得出来得结果是

       key: kCBAdvDataIsConnectable, value: 1

       key: kCBAdvDataLocalName, value: SimpleBLEPeripheral

       key: kCBAdvDataServiceUUIDs

          uuid(0): FF F0

       key: kCBAdvDataTxPowerLevel, value: 0

    我想获取得广播数据还是读取不到。。。。

  • 对于iOS设备,我是通过kCBAdvDataServiceUUIDs得到广播数据的。

  • Li Zongwu:

    我也感觉广播数据应该是在advertisementData中的,可以里面就是没有kCBAdvDataServiceUUIDs这个键值。纠结。。。。不知道是不是CC2540那里面的程序不对,你的

    -(void)centralManagerDidUpdateState:(CBCentralManager *)central

    {....}这里面怎么定义的啊。。。

  • 用我之前提供的代码,就可以得到kCBAdvDataServiceUUIDs这个key值,这个key值对应的就是广播里地所谓的数据了。

  • 楼主你好,我现在也遇到了同样的问题,请问,后来这个问题你解决了么?哪里可以找到advdata啊?

  • 楼上的兄弟,问题解决了吗?我也正在整这个问题。能否共同探讨一下?QQ952580941