Other Parts Discussed in Thread: CC2640R2F,
在cc2640R2F或cc2642R1F的SDK中,通常用
Mac0 = HWREG(FCFG1_BASE + FCFG1_O_MAC_BLE_0);
Mac1 = HWREG(FCFG1_BASE + FCFG1_O_MAC_BLE_1);
来获取芯片MAC地址,在CC2340R5中这样似乎不行。应该怎么获取呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该是量产版吧?用的是CCS Resource Explorer里下载的CC2340R5最新SDK
我已经读到了Mac地址。
包含头文件#include <ti/devices/cc23x0r5/inc/hw_fcfg.h>
uint8_t MacAddress[6];
MacAddress[5] = fcfg->deviceInfo.bleAddr[0];
MacAddress[4] = fcfg->deviceInfo.bleAddr[1];
MacAddress[3] = fcfg->deviceInfo.bleAddr[2];
MacAddress[2] = fcfg->deviceInfo.bleAddr[3];
MacAddress[1] = fcfg->deviceInfo.bleAddr[4];
MacAddress[0] = fcfg->deviceInfo.bleAddr[5];
您好,
量产版读Mac address的代码如下:
#include <string.h>
#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(inc/hw_fcfg.h)
uint8_t bleAddressRead[6] = {0};
// fcfg->deviceInfo.bleaddr is little-endian
memcpy(bleAddressRead, fcfg->deviceInfo.bleAddr, 6);
// Print the address
MenuModule_printf(APP_MENU_PROFILE_STATUS_LINE4, 0, "bleAddressRead = 0x%x%x%x%x%x%x",
bleAddressRead[5], bleAddressRead[4], bleAddressRead[3],
bleAddressRead[2], bleAddressRead[1], bleAddressRead[0]);
注意这样读出来的地址是小的在前的,所以打印显示的时候bleAddressRead[5]在最前面,bleAddressRead[0]在最后。