This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: CC2642R: GATT_ExchangeMTU更改MTU失败

Part Number: CC2642R
Other Parts Discussed in Thread: SYSCONFIG

SDK版本:simplelink_cc13xx_cc26xx_sdk_7_10_00_98(最新版本)

硬件:自制最小系统板5287.原理图 蓝牙模块-CC2642_V1.3.pdf

现象:

使用TI的simple_central和simple_peripheral测试,主机扫描到从机,建立连接后,会调用GATT_ExchangeMTU更新MTU:

static void SimpleCentral_startSvcDiscovery(void)
{

    bStatus_t status;
    attExchangeMTUReq_t req;

    // Initialize cached handles
    svcStartHdl = svcEndHdl = 0;

    discState = BLE_DISC_STATE_MTU;

    // Discover GATT Server's Rx MTU size
    req.clientRxMTU = scMaxPduSize - L2CAP_HDR_SIZE;
    // ATT MTU size should be set to the minimum of the Client Rx MTU
    // and Server Rx MTU values
    //VOID GATT_ExchangeMTU(scConnHandle, &req, selfEntity);
    status = GATT_ExchangeMTU(simpleBLEConnHandle, &req, selfEntity);
    if(status == 0){
        sprintf(printbuf,"Request was queued successfully.\r\n");
    }else{
        sprintf(printbuf,"Error:status=%d.\r\n",status);
    }
    PRINT_LOG;

}

 SimpleCentral_processGATTMsg(gattMsgEvent_t *pMsg)函数中收到ATT_MTU_UPDATED_EVENT情况非常少见,大部分情况是收不到,在收不到ATT_MTU_UPDATED_EVENT的情况下,连接会自动断开。

GATT_ExchangeMTU()函数的返回状态是0,即成功,我尝试更新的 ATT MTU 大小的值是65,这是工程默认可改MTU的最大值。

simple_peripheral用手机连接改MTU每次都是正常的。此问题应该与simple_peripheral无关。

x 出现错误。请重试或与管理员联系。