This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: 修改分区划分疑问

Part Number: LAUNCHXL-CC26X2R1

我的诉求:user application划分分区为0-0x28000(160k), persistent0x28000 -0x50000(160K),  bim_onchip(8k), ccfg+NV(24k), 总计352k

且user application可以读写persistent和ccfg+NV(24k)分区

persistent可以读写user application和ccfg+NV(24k)分区

bim_onchip可以读写user application和ccfg+NV(24k)分区

我应如何修改?

自己测试如下

工程:persistent

1、

2、

3、

4、报错

makefile:184: recipe for target 'persistent app_CC26X2R1_LAUNCHXL_tirtos7_ticlang.out' failed
error #10324-D: BOUND section ".TI.bound:flashBuf0" spans the boundary of an existing memory range FLASH_IMG_HDR
error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".TI.bound:flashBuf0" size 0x28000
error #10010: errors encountered during linking; "persistent app_CC26X2R1_LAUNCHXL_tirtos7_ticlang.out" not built