Part Number: CC2652P7
Other Parts Discussed in Thread: UNIFLASH
根据芯片的设计手册与参考设计在自己的板子上进行了设计,上电后发现DCOUPL与DCDC_SW的输出与手册中的要求不符合,DCDC_SW只有一点几V并且会缓慢下降,DCOUPL只有0.2V左右,使用uniflash烧写代码时会出现 (Error -2131 @ 0x0) Unable to access device register如下错误。请问应该如何解决
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请从以下步骤进行问题定位:
1.使用uniflash工具时,是否可以显示如下图标:

2.使用programmer 2 工具时,是否可以查看到芯片型号。
3.是否已经安装xds110驱动。
如果以上都正常显示并工作,
麻烦您可以在以下链接申请相应的硬件审核:SIMPLELINK-2-4GHZ-DESIGN-REVIEWS,有专业的硬件工程师帮您查看相应硬件问题。
您好,使用uniflash可以看到如图界面,但是使用programmer2不能识别到芯片。感觉像是芯片没有启动,DCDC_SW与DCOUPL的值都不正确
您好,这属于您这边的硬件电路设计问题
麻烦您可以在以下链接申请相应的硬件审核:SIMPLELINK-2-4GHZ-DESIGN-REVIEWS,有专业的硬件工程师帮您查看相应硬件问题。