知道ti的ble芯片都有一个唯一的48bit的地址,请问一下有没有什么方法可以将这个唯一的48bit的地址转换成唯一的32bit的地址呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Each CC2540 is programmed with a unique 48-bit MAC address. This is contained in the information page and can't be changed.
hi susan yang
我在网上百度了一下mac地址的组成:
MAC(Medium/Media Access Control)地址,用来表示互联网上每一个站点的标识符,采用十六进制数表示,共六个字节(48位)。其中,前三个字节是由IEEE的注册管理机构RA负责给不同厂家分配的代码(高位24位),也称为“编制上唯一的标识符”(Organizationally Unique Identifier),后三个字节(低位24位)由各厂家自行指派给生产的适配器接口,称为扩展标识符(唯一性)。
我的理解是同一生产商,高24位的mac地址是一样的,低24位的mac地址不同。也是就是所有ti的cc2541芯片的mac地址的高24bit都是相同的。
不知道ti的这个蓝牙芯片是不是也是遵循这个规则的?