Other Parts Discussed in Thread: CC2651P3
使用的是LP-CC2651P3开发板,片上flash大小为352kb,考虑到蓝牙协议栈和应用程序的大小,感觉空间有点局促,请问可以进行蓝牙的片上oad 吗?有文档或例程可以参考一下吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用的是LP-CC2651P3开发板,片上flash大小为352kb,考虑到蓝牙协议栈和应用程序的大小,感觉空间有点局促,请问可以进行蓝牙的片上oad 吗?有文档或例程可以参考一下吗?
谢谢你的回复!但我想你可能还不太清楚我的问题,我使用的是CC2651P3芯片开发板,SDK版本为simplelink_cc13xx_cc26xx_sdk_6_30_00_84,之前根据文档https://dev.ti.com/tirex/content/simplelink_cc13xx_cc26xx_sdk_6_30_00_84/docs/ble5stack/ble_user_guide/html/quickstart-guide/ble5-quick-start.html#using-ble5-stack-projects-with-ccs
所描述的步骤,使用(project_zero)示例,已经走通了oad_offchip的步骤,但考虑到我们的产品是没有外挂flash的,所以询问关于CC2651P3芯片的oad_onchip功能,看过你之前给的回复的文档中有关于oad_onchip的步骤,也打算照着文档所描述的步骤去走一遍,但我在CC651P3的官方SDK里并没有找到文档里进行oad_onchip所使用的(simple_peripheral_oad_onchip)和(persistent_app)这两个例程,所以没法照着文档的里的步骤去实现。因此我想问是否有我所使用的CC2651P3芯片的蓝牙“片上”oad的示例和具体实现步骤呢?
很感谢你的回复,你所提供的帖子中的,Option 1和Option 2两个蓝牙OAD的方案我试着走,并且走通了,但我发现这两个方案都是使用片外flash的OAD,并不是用片上flash的OAD。
根据OAD所使用的.bin文件的大小为180kb左右,但CC651P3的片上的flash空间仅有352kb推断,片上flash似乎不足以放下一个应用程序和一个需要OAD升级的程序,是不是CC651P3就没法进行片上flash的OAD,还是说有什么特别的方式进行片上OAD?
Click here to get other payment method
Tip:Please refresh the page after the payment is successful
We will gradually support it
根据OAD所使用的.bin文件的大小为180kb左右,但CC651P3的片上的flash空间仅有352kb推断,片上flash似乎不足以放下一个应用程序和一个需要OAD升级的程序,是不是CC651P3就没法进行片上flash的OAD
正如您所说的,不足以您进行片上oad。有一种方案是,一边擦除一边写入,您有了解过吗。具体的方案需要您去制定,我这边为您提供思路,不知道是否对您有帮助。
好的!谢谢你的回复!我觉得很有帮助。
Click here to get other payment method
Tip:Please refresh the page after the payment is successful
We will gradually support it