This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
此帖为TI 的Bluetooth 方案一些常见问题的FAQ 解答,希望能对大家有所帮助。
一些重复提问一些常见问题,将会在这里陆续更新。
1. 通用问题:
http://e2e.ti.com/support/wireless_connectivity/f/538/t/337412
2. CC2640/50 问题:
http://e2e.ti.com/support/wireless_connectivity/f/538/t/404236
3. TI BLE在IOS,Android的数据传输率 问题:
http://www.deyisupport.com/question_answer/wireless_connectivity/bluetooth/f/103/t/108802.aspx
4. CC2640 片外OAD 问题:
http://www.deyisupport.com/question_answer/wireless_connectivity/bluetooth/f/103/t/108589.aspx
有关CC2640/50在SimpleBLEPeripheral工程中添加uart会影响蓝牙广播的问题,发布下吧,等待中
你好,我看到您在一个关于CC2640的ADC的帖子中回复了,我试验了您的代码,发现采集到的数会变,但是IO口的对应好像不对,您能不能发一下关于AUX_IO和芯片IO以及内部输入的对应关系呢。谢谢。
想请教您一个问题,我在用CC2541 ADC采集外部电压时,用内部1.25V参考,差分通道,12位分表率,结果偏高。外部电路是经过电阻分压之后的,电阻精度是0.1%,实际电压是12.12,程序转换后的采集结果是12.45,误差有点大,是什么原因呢?然后我换成AVDD5引脚做参考电压,测量结果基本正常