This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: MAP文件疑问

Part Number: LAUNCHXL-CC26X2R1

1、RTOS_SRAM和SRAM区别是什么?

2、为什么SRAM的length不是手册上的80K而是76K?

  • 您好,

    1.RTOS_SRAM是专门用于实时操作系统(RTOS)的存储器,它通常用于运行RTOS的代码和数据,包括任务堆栈、中断向量等。其特点是速度快、响应时间短,能够满足实时操作系统对内存访问的即时需求。

    SRAM则是普通的静态随机存取存储器,用于存取程序代码、数据和临时变量等。

    区别在于:RTOS_SRAM是专门为实时操作系统设计的存储器,用于处理实时任务和中断,具有快速响应的特点;而SRAM是通用的存储器,用于存储程序代码和数据,不具备RTOS_SRAM的实时性能。

    2.在实际运用中,由于一些系统和硬件需要一部分SRAM的空间,因此可能会小于数据手册的值。空间的部分占用得以保证系统正常运行。

    希望对您有所帮助。