This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想自己做蓝牙设备,CC2541BLE低功耗模式,需要用到两个晶振吗?
不需要,但是两个晶振一个提供快速处理能力,比如12M,另外一个可以提供时钟级32768,同时32768由于频率低可以更好的进行降低功耗,所以最好使用两个,这个可以程序里面自主选择模式,休眠状态或者不需要太快速处理时候就使用低频的32768,还能更好的提供时间基准。
这个所谓是的快速处理是指多长时间一个指令周期?或者说我只用32.768K晶振可以正常的传输数据吗?
http://pan.baidu.com/s/1bnCQVuB
给你一些我的学习资料。希望帮到你,本来想传上来呢,有大小限制。
是个好东西,其实我有的,但是之前没做这个,现在要用到了,手头也没有板子了,现在就是想确定能不能只用那个32.768的晶振,把板子做小!!
方便加下你的扣扣吗?哥们。。。