This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

设置keyfob的连接超时时间即Supevision Timeout无效



我直接将KeyFobApp_Init的以下参数修改为:

uint16 desired_min_interval = 32; //40ms
uint16 desired_max_interval = 48; //60ms
uint16 desired_slave_latency = 0;
uint16 desired_conn_timeout = 20; //200ms

设置后,当KeyFob远离主设备(手机)时,并没有立刻报警,大概过了10s中才报警,感觉设备这几个时间没有效果?

另外,slave和master之间的隔connect interval时间会发送connect event,这个connect event是slave发送的吗?app是否能捕获这个消息,或者这个消息master的回应?

  • slave和master之间的隔connect interval时间会发送connect event,这个connect event是否就是param update,是slave发送的吗?app是否能捕获这个消息,或者这个消息master的回应?

    这个问题有人回答下吗?