This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 如何输出固定数量的PWM脉冲

Part Number: CC2640R2F


我能使用CC2640R2F输出PWM脉冲,但是如何输出固定数量的PWM脉冲呢?

  • 如何输出固定数量的PWM脉冲

    为您提供两个方向:

    1.需要编程控制CC2640R2F的GPIO口生成所需的脉冲序列

    2.还可以考虑使用CC2640R2F的硬件定时器来生成精确的PWM脉冲

    您现在是用什么方式来输出PWM呢?

  • 我现在输出PWM的方法如下,如何修改才能输出固定数量的PWM脉冲?
    比如我想输出10个PWM脉冲数(其中包含高脉冲和低脉冲)

    //生成微秒PWM方波
    int pwm()
    {
    // Import PWM Driver definitions
    //#include <ti/drivers/PWM.h>

    PWM_Handle pwm;
    PWM_Params pwmParams;
    uint32_t dutyValue;
    // Initialize the PWM driver.
    PWM_init();
    // Initialize the PWM parameters
    PWM_Params_init(&pwmParams);
    pwmParams.idleLevel = PWM_IDLE_LOW; // Output low when PWM is not running
    pwmParams.periodUnits = PWM_PERIOD_HZ; // Period is in Hz
    pwmParams.periodValue = 1e6; // 1MHz (1e6 = 1000000), 1us
    pwmParams.dutyUnits = PWM_DUTY_FRACTION; // Duty is in fractional percentage
    pwmParams.dutyValue = 0; // 0% initial duty cycle

    // Open the PWM instance
    pwm = PWM_open(Board_PWM0, &pwmParams); // PWM0输出PWM到引脚GPIO6
    //pwm = PWM_open(Board_PWM1, &pwmParams); // PWM1输出PWM到引脚GPIO7

    if (pwm == NULL) {
    return 0;
    // PWM_open() failed
    //while (1);
    }


    PWM_start(pwm); // start PWM with 0% duty cycle

    //计算占空比
    dutyValue = (uint32_t) (((uint64_t) PWM_DUTY_FRACTION_MAX * 50) / 100);
    PWM_setDuty(pwm, dutyValue); // set duty cycle to 50%

    return 1;
    }

  • Hi Zhongxin,

    您可以考虑通过配置定时器来跟踪生成的脉冲数量,代码里可以加一个生成PWM脉冲循环(<10),等待定时器超时。

  • 不客气,欢迎随时来论坛交流!