Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: CC2340R5
在GitHub上找到一份throughput相关的代码(github.com/.../throughput_peripheral)
计划移植到simplelink_lowpower_f3_sdk_7_20_00_29的data_stream示例,用于测试CC2340R5的吞吐量。
在BLEAppUtil_init里调用了ThroughputPeripheral_createTask,但是目前程序会卡在ThroughputPeripheral_taskFxn里的第一个EventP_pend。
请问是我哪里流程错了吗?
部分代码如下:
void BLEAppUtil_init(ErrorHandler_t errorHandler, StackInitDone_t initDoneHandler,
BLEAppUtil_GeneralParams_t *initGeneralParams,
BLEAppUtil_PeriCentParams_t *initPeriCentParams)
{
// Register the application error handler
errorHandlerCb = errorHandler;
// Register the init done handler - will be called from the GAP_DEVICE_INIT_DONE_EVENT
appInitDoneHandler = initDoneHandler;
// Assign the BLEAppUtil parameters from the user to the local parameters
BLEAppUtilLocal_GeneralParams = initGeneralParams;
BLEAppUtilLocal_PeriCentParams = initPeriCentParams;
// Create a message queue for message to be sent to BLEAppUtil
BLEAppUtil_createQueue();
// Create BLE stack task
bleStack_createTasks();
// Create local app task
BLEAppUtil_createBLEAppUtilTask();
ThroughputPeripheral_createTask();
// Construct a mutex that will be used by the following functions:
// BLEAppUtil_registerEventHandler
// BLEAppUtil_unRegisterEventHandler
// BLEAppUtil_callEventHandler
pthread_mutex_init(&mutex, NULL);
}
int ThroughputPeripheral_createTask(void)
{
int retVal = 0;
pthread_attr_t param_attribute;
struct sched_param param;
retVal = pthread_attr_init(¶m_attribute);
param.sched_priority = TP_TASK_PRIORITY;
retVal |= pthread_attr_setschedparam(¶m_attribute, ¶m);
retVal |= pthread_attr_setstack(¶m_attribute, tpTaskStack, TP_TASK_STACK_SIZE);
retVal |= pthread_attr_setdetachstate(¶m_attribute, PTHREAD_CREATE_DETACHED);
retVal |= pthread_create(&tpTask,
¶m_attribute,
&ThroughputPeripheral_taskFxn,
NULL);
return retVal;
}
static void *ThroughputPeripheral_taskFxn(void *arg)
{
// Initialize application
ThroughputPeripheral_init();
// Application main loop
for (;;)
{
uint32_t events;
// Waits for an event to be posted associated with the calling thread.
// Note that an event associated with a thread is posted when a
// message is queued to the message receive queue of the thread
events = EventP_pend(syncEvent, TP_ALL_EVENTS, UTIL_EVENT_ID_NONE,
ICALL_TIMEOUT_FOREVER);