This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: TX Power Index

Part Number: CC2340R5


关于CC2340R5的TX_Power_Index问题,我逛论坛发现七八个月前就已经修复好了这个问题,我现在使用的SDK版本是7.20.0.29,发现仍然不可以调用,最新的7.20.1.10也是一样的?请问我需要修改时,应该怎样操作?

/**
 * @defgroup TX_Power_Index TX Power Index
 * @{
 */
#ifndef CC23X0
#if defined( CC26XX ) || defined( CC13XX ) || defined ( CC33xx )
#define HCI_EXT_TX_POWER_MINUS_20_DBM                   LL_EXT_TX_POWER_MINUS_20_DBM            //!< -20 dBm
#define HCI_EXT_TX_POWER_MINUS_18_DBM                   LL_EXT_TX_POWER_MINUS_18_DBM            //!< -18 dBm
#define HCI_EXT_TX_POWER_MINUS_15_DBM                   LL_EXT_TX_POWER_MINUS_15_DBM            //!< -15 dBm
#define HCI_EXT_TX_POWER_MINUS_12_DBM                   LL_EXT_TX_POWER_MINUS_12_DBM            //!< -12 dBm
#define HCI_EXT_TX_POWER_MINUS_10_DBM                   LL_EXT_TX_POWER_MINUS_10_DBM            //!< -10 dBm
#define HCI_EXT_TX_POWER_MINUS_9_DBM                    LL_EXT_TX_POWER_MINUS_9_DBM             //!< -9 dBm
#define HCI_EXT_TX_POWER_MINUS_6_DBM                    LL_EXT_TX_POWER_MINUS_6_DBM             //!< -6 dBm
#define HCI_EXT_TX_POWER_MINUS_5_DBM                    LL_EXT_TX_POWER_MINUS_5_DBM             //!< -5 dBm
#define HCI_EXT_TX_POWER_MINUS_3_DBM                    LL_EXT_TX_POWER_MINUS_3_DBM             //!< -3 dBm
#define HCI_EXT_TX_POWER_0_DBM                          LL_EXT_TX_POWER_0_DBM                   //!< 0 dBm
#define HCI_EXT_TX_POWER_1_DBM                          LL_EXT_TX_POWER_1_DBM                   //!< 1 dBm
#define HCI_EXT_TX_POWER_2_DBM                          LL_EXT_TX_POWER_2_DBM                   //!< 2 dBm
#define HCI_EXT_TX_POWER_3_DBM                          LL_EXT_TX_POWER_3_DBM                   //!< 3 dBm
#define HCI_EXT_TX_POWER_4_DBM                          LL_EXT_TX_POWER_4_DBM                   //!< 4 dBm
#define HCI_EXT_TX_POWER_5_DBM                          LL_EXT_TX_POWER_5_DBM                   //!< 5 dBm
#if defined( CC13X2P ) || defined( CC33xx )
#define HCI_EXT_TX_POWER_P2_14_DBM_P4_6_DBM             LL_EXT_TX_POWER_P2_14_DBM_P4_6_DBM      //!< P2: 14 dBm P4: 6 dBm
#define HCI_EXT_TX_POWER_P2_15_DBM_P4_7_DBM             LL_EXT_TX_POWER_P2_15_DBM_P4_7_DBM      //!< P2: 15 dBm P4: 7 dBm
#define HCI_EXT_TX_POWER_P2_16_DBM_P4_8_DBM             LL_EXT_TX_POWER_P2_16_DBM_P4_8_DBM      //!< P2: 16 dBm P4: 8 dBm
#define HCI_EXT_TX_POWER_P2_17_DBM_P4_9_DBM             LL_EXT_TX_POWER_P2_17_DBM_P4_9_DBM      //!< P2: 17 dBm P4: 9 dBm
#define HCI_EXT_TX_POWER_P2_18_DBM_P4_10_DBM            LL_EXT_TX_POWER_P2_18_DBM_P4_10_DBM     //!< P2: 18 dBm P4: 10 dBm
#define HCI_EXT_TX_POWER_P2_19_DBM                      LL_EXT_TX_POWER_P2_19_DBM               //!< P2: 19 dBm
#define HCI_EXT_TX_POWER_P2_20_DBM                      LL_EXT_TX_POWER_P2_20_DBM               //!< P2: 20 dBm
#endif // CC13X2P || CC33xx
#else // CC254x
#define HCI_EXT_TX_POWER_MINUS_23_DBM                  LL_EXT_TX_POWER_MINUS_23_DBM //!< -23 dBm
#define HCI_EXT_TX_POWER_MINUS_6_DBM                   LL_EXT_TX_POWER_MINUS_6_DBM  //!< -6 dBm
#define HCI_EXT_TX_POWER_0_DBM                         LL_EXT_TX_POWER_0_DBM        //!< 0 dBm
#define HCI_EXT_TX_POWER_4_DBM                         LL_EXT_TX_POWER_4_DBM        //!< 4 dBm
#endif // CC26XX/CC13XX
#endif //CC23X0
/** @} End TX_Power_Index */