This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R-Q1: 实现连续扫描

Part Number: CC2642R-Q1


GapScan_enable的描述中,三个参数都为0应该可以实现连续扫描,实际值扫描一个period就停止了,是哪里的问题?

  • 您好,

    您可以查看 Simple Link Academy 处理广告和扫描的基础实验中 Task 3 中描述了 GapScan_enable 函数的正确用法:

    // === SOLUTION [Scan indefinitely] ===
    //Scan period. Ignored if duration is zero. 1.28 sec unit
    uint16_t scanPeriod = 4; // 4 * 1.28 s = 5.12 s.
    GapScan_enable(scanPeriod, DEFAULT_SCAN_DURATION, 0);
    // ==== END SOLUTION ====