Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG
使用的是SDK版本为 simplelink_lowpower_f3_sdk_7_10_00_35,如何使芯片进入睡眠模式,可以提供一下芯片进入睡眠与唤醒的例程吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考这个例程没问题:C:\ti\simplelink_lowpower_f3_sdk_7_40_00_64\examples\rtos\LP_EM_CC2340R5\drivers\gpioshutdown
请问具体是什么错误?
我还是使用simplelink_lowpower_f3_sdk_7_10_00_35这个SDK,就是使用Power_shutdown(0, 0);这个API后下载程序时出现了 Error connecting to the target: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again. (Emulation package 9.10.0.00080) 错误。没有Power_shutdown(0, 0);这个API时正常。
您好,
需要将 SDK 更新到最新版本 7_40_00_64 。
是调用Power_shutdown(0, 0)之后出现Error -615吗?那是正常的啊,芯片进入shutdown模式了,是不能在线调试的。
验证shutdown生效的方法参见shutdown例程的readme文档:
Best regards,
Shuyang
在CCS中,Window -> Preference -> Code Composer Studio -> Products,点击Refresh刷新一下,应该可以检索到sysconfig 1.18.1
Best regards,
Shuyang