Part Number: CC2642R
使用UART2出现如下问题,有什么相应的解决方法吗
UART2_Params params;
UART2_Params_init(¶ms);
params.baudRate = 115200;
params.readMode = UART2_Mode_BLOCKING;
params.writeMode = UART2_Mode_BLOCKING;
// Open the UART
UART2_Handle uart;
uart = UART2_open(0, ¶ms);
// Enable receiver, inhibit low power mode
UART2_rxEnable(uart);
// Read from the UART.
size_t bytesRead;
uint8_t buffer[4];
int32_t status;
status = UART2_read(uart, buffer, 4, &bytesRead); // status为-9
/*!
* @brief The UART is currently in use.
*/
// #define UART2_STATUS_EINUSE (-9)