Part Number: CC2642R
Other Parts Discussed in Thread: SYSCONFIG
工程内配置的串口CONFIG_DISPLAY_UART是BT_UART_RX和BT_UART_TX吗
现在串口CONFIG_DISPLAY_UART,不能打开
目前想要打开BT_UART_RX和BT_UART_TX串口,应该如何配置


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1.CONFIG_DISPLAY_UART是用于控制与外部显示设备的串口通信,
BT_UART_RX和BT_UART_TX是蓝牙UART通信的引脚
2.
你试试在sysconfig里面打开配置


默认情况下、UART Rx/TX/CTS/RTS 引脚为 DIO_2/DIO3/DIO_19/DIO_18
你不是要打开BT_UART_RX和BT_UART_TX串口吗?
不配置到这个引脚 试试
CONFIG_DISPLAY_UART使用的就是XDS
使用的官方的程序simple_peripheral_CC26X2R1_LAUNCHXL_tirtos7_ticlang,目前想的是把BT_UART_RX和BT_UART_TX的数据读到fff5,然后通过无线接收fff5