This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540传输速率测试

Other Parts Discussed in Thread: CC2540

您好,

在做CC2540数据传输速率测试的时候,数据接收使用Device Monitor + USB dongle,发送方式采用Notification方式,发送数据5000包,每包20字节,协议栈的版本为1.4.0。

1 发送间隔设置为10ms,1包/次,interval为6,不出现丢包的情况,发送速率2KB/s,接收速率2KB/s。

2 发送间隔设置为10ms,2包/次,interval为6,接收3301包,发送速率4KB/s,接收速率2.4KB/s,丢包34%。

3 发送间隔设置为15ms,3包/次,interval为6,接收1601包后,器件程序死掉了。

4 发送间隔设置为20ms,2包/次,interval为6,接收5000包,发送速率2KB/s,接收速率2KB/s,丢包0%。

5 发送间隔设置为20ms,3包/次,interval为6,接收4114包,发送速率3KB/s,接收速率2.5KB/s,丢包18%。

所以请问,我的问题是:

1 使用电脑的Device Monitor的接收速率是不是只能达到这个速率,手机APP会提升速率?

2 如果不是的话,请问我该如何提升传输速率,因为官方文档给出的参考速率是5.9KB/s?

  • Hao,

    你可以参考一下这个:http://processors.wiki.ti.com/index.php/CC2540_Data_Throughput

    USB dongle 和PC工具的配套不排除能力有限。

    不行的话你可以用手机做master测试一下,最好用Android手机,iOS限制太大。