Part Number: CC2642R
环境:simplelink_cc13xx_cc26xx_sdk_7_40_00_77
示例:simple_central
关于特征值发现过程的疑问点:
在SimpleCentral_processGATTDiscEvent中处理特征值发现的时候,需要将成功发现到的特征值charHandle进行存储,用于后续的特征值读写,如下面语句:
else if (discState == BLE_DISC_STATE_CHAR)
{
// Characteristic found, store handle
if ((pMsg->method == ATT_READ_BY_TYPE_RSP) &&
(pMsg->msg.readByTypeRsp.numPairs > 0))
{
uint8_t connIndex = SimpleCentral_getConnIndex(scConnHandle);
// connIndex cannot be equal to or greater than MAX_NUM_BLE_CONNS
SIMPLECENTRAL_ASSERT(connIndex < MAX_NUM_BLE_CONNS);
// Store the handle of the simpleprofile characteristic 1 value
connList[connIndex].charHandle
= BUILD_UINT16(pMsg->msg.readByTypeRsp.pDataList[3],
pMsg->msg.readByTypeRsp.pDataList[4]);
... ...
}
discState = BLE_DISC_STATE_IDLE;
}
其中存储特征值charHandle的时候:
connList[connIndex].charHandle = BUILD_UINT16(pMsg->msg.readByTypeRsp.pDataList[3], pMsg->msg.readByTypeRsp.pDataList[4]);
pDataList中数据对应的格式是怎样的?为什么pDataList[3]和pDataList[4]组成了charHandle?关于这个问题,哪里有文档说明?或者代码上有相关定义吗?