This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

iphone app 如何修改蓝牙设备的Interval ,slave latency等参数



1 能否实现在app运行时用代码修改这些参数,来实现关闭低功耗

 环境: 双模蓝牙接到串口中,发送参数速率 每隔5ms 发送9个字节 && 每隔1是发送20个字节 &&每隔1.5s 发送10个字节

       这样速率下 导致很多数据延迟 或者丢失了某几个字节, 出现连续20个0的情况

 这个是否可以通过修改 interval  slave latency 和timeout 来修正上述问题??

2 ios ble 在收发数据时  完全通过一个character 来write without response && noticfy 

                                       或者通过一个character 来write withou  ,另一个 character 来noticfy。

上述两种情况 是否影响高速收发数据时速度?