This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: CCStudio 20.0.0使用J-Link烧录报错

Part Number: CC2340R5

我使用J-Link连接到CC2340R5 LaunchPad,使用CCS编译simplelink_lowpower_f3_sdk_8_20_00_119里面的examples\nortos\LP_EM_CC2340R5\drivers\empty,编译成功,选择SEGGER J-Link Emulator,在Flash Project的时候发生错误,具体log输出如下所示,请帮忙看看是什么问题,谢谢!

Debug Output:

Trouble Writing Memory Block at 0x4e020000 on Page 0 of Length 0x800: Flash download failed! ...
File Loader: Verification failed: Target failed to write 0x4E020000
GEL: File: C:\Users\ks\AppData\Local\Temp\ti_cloud_storage\empty_LP_EM_CC2340R5_nortos_ticlang.out: Load failed.
Error: Stat [ JLINKARM_IsHalted() call ] failed!
Trouble Halting Target CPU: Halt failed!
Error: Stat [ JLINKARM_IsHalted() call ] failed!
Trouble Halting Target CPU: Halt failed!
Error: Stat [ JLINKARM_IsHalted() call ] failed!