您好,自己用CC2340R52E0RGE设计了电路板,图纸如下
问题(1)目前下载程序及运行程序都正常,电感L20换的10uh,外部供电VDD_BT=3.3V, VDDD=1.28V正常, 但是DCDC 输出端口VDCDC用万用表测量只有1.49V,跟手册描述的不一样,
,手册里面的是3.0v,低于2。2v会自动切换到LDO,模式,而且例程里面已经开启配置位DCDC模式,
,请问这个问题VDCDC=1.49V的原因是什么?问题(2)用xds110下载程序部正常,用jtag下载程序正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,自己用CC2340R52E0RGE设计了电路板,图纸如下
问题(1)目前下载程序及运行程序都正常,电感L20换的10uh,外部供电VDD_BT=3.3V, VDDD=1.28V正常, 但是DCDC 输出端口VDCDC用万用表测量只有1.49V,跟手册描述的不一样,
,手册里面的是3.0v,低于2。2v会自动切换到LDO,模式,而且例程里面已经开启配置位DCDC模式,
,请问这个问题VDCDC=1.49V的原因是什么?问题(2)用xds110下载程序部正常,用jtag下载程序正常。
按照下方FAQ再重新试一下。
感谢您的回复,再TRM里面找到这段话,
The input supply of DCDC can range from 2.2V to 3.8V. DCDC regulates the output to 1.5V. But for GLDO, the
supply can range from 1.71V to 3.8V to generate a regulated output of 1.5V. DCDC hardware is designed so
that when the supply voltage drops below 2.2V, DCDC automatically shuts off and only GLDO generates the
regulated VDDR. 所以来看1.5V是正常的。您看下是不是这样?