This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: CC2340R5 Custom BLE PHY: How to transmit raw/custom BLE advertising PDUs without BLE stack using prop_rf/rfPacketTx?

Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG

Hi,

I am trying to use the CC2340R5 with the LP_EM_CC2340R5/prop_rf/rfPacketTx example as a starting point.

My goal is:

  • Use the Custom RF stack configuration with BLE PHY selected (Generic 1 Mbps / 2 Mbps / Coded)

  • Transmit a fixed custom BLE advertising PDU

  • Do not use the full BLE stack (GAP/GATT/LL)

  • Later switch dynamically between BLE PHY and other PHYs for a multi-protocol application

Currently I can run with the prop_rf example, but I cannot make a valid BLE advertising packet that can be detected by a phone or nRF Connect.

I would like to understand:

  1. When using Custom -> BLE PHY in SysConfig, does the radio automatically handle:

    • BLE Access Address (0x8E89BED6)

    • CRC24

    • Data whitening

    • BLE bit ordering

  2. Is it sufficient to provide only the BLE advertising PDU payload:

    • Header

    • AdvA

    • AdvData

or do I need to manually construct the full BLE over-the-air packet?

  1. Does the rfPacketTx example use a proprietary packet formatter that prepends packet length or uses a non-BLE packet structure?

  2. Is there an official example for transmitting raw/custom BLE advertising packets without using the BLE stack?

My current intention is to transmit only on advertising channel 37 (2402 MHz) first.

Thank you.

  • Hello, we have received your case and the investigation will take some time. Thank you for your patience.

  • static void ble_build_adv_pdu(void)
    {
      // --- PDU Header ---
      ble_pdu_raw[0] = 0x42;  // ADV_NONCONN_IND (0x02) | TxAdd=1 (0x40)
      ble_pdu_raw[1] = 15;    // Length: 6 (AdvA) + 3 (Flags) + 6 (Name) = 15
    
      // --- AdvA: Random Static Address CC:66:55:44:33:22 (LSByte first) ---
      ble_pdu_raw[2] = 0x22;
      ble_pdu_raw[3] = 0x33;
      ble_pdu_raw[4] = 0x44;
      ble_pdu_raw[5] = 0x55;
      ble_pdu_raw[6] = 0x66;
      ble_pdu_raw[7] =
        0xCC;  // MSByte: bits 7:6 = '11' (Random Static).You can edit any byte of address except this bits 7:6!
    
      // --- AD Structure 1: Flags ---
      ble_pdu_raw[8]  = 0x02;  // AD Length
      ble_pdu_raw[9]  = 0x01;  // AD Type: Flags
      ble_pdu_raw[10] = 0x06;  // LE General Discoverable | BR/EDR Not Supported
    
      // --- AD Structure 2: Complete Local Name "FG22" ---
      ble_pdu_raw[11] = 0x05;  // AD Length
      ble_pdu_raw[12] = 0x09;  // AD Type: Complete Local Name
    
    
      ble_pdu_raw[13] = '2';
      ble_pdu_raw[14] = '3';
      ble_pdu_raw[15] = '4';
      ble_pdu_raw[16] = '0';
    
      memcpy(ble_pdu_send+1,ble_pdu_raw,17);
      
      ble_pdu_send[0]=17;
    
    }
    
    /***** Callback Functions *****/
    void defaultCallback(RCL_Command *cmd, LRF_Events lrfEvents, RCL_Events rclEvents)
    {
        if (rclEvents.lastCmdDone)
        {
            gCmdDone += 1;
    
            GPIO_toggle(CONFIG_GPIO_GLED);
        }
    }
    
    /***** Function definitions *****/
    
    void *mainThread(void *arg0)
    {
        /* Initialize and open RCL */
        RCL_init();
    
        RCL_Handle rclHandle = RCL_open(&rclClient, &LRF_config);
    
        /* Set RF frequency */
        rclPacketTxCmdGenericTx.rfFrequency = FREQUENCY;
    
        /* Start command as soon as possible */
        rclPacketTxCmdGenericTx.common.scheduling = RCL_Schedule_Now;
        rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle;
    
        rclPacketTxCmdGenericTx.config.fsOff = FS_OFF; // Turn off FS
    
        /* Callback triggers on last command done */
        rclPacketTxCmdGenericTx.common.runtime.callback = defaultCallback;
        rclPacketTxCmdGenericTx.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value;
    
        /* Set RCL TX buffer packet to be packet buffer */
        RCL_Buffer_TxBuffer *txPacket = (RCL_Buffer_TxBuffer *)&packet;
    
        GPIO_setConfig(CONFIG_GPIO_GLED, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
        GPIO_write(CONFIG_GPIO_GLED, CONFIG_GPIO_LED_OFF);
    
        ble_build_adv_pdu();
    
        while(1)
        {
            /* Create packet with random payload */
            uint8_t *txData;
            txData = RCL_TxBuffer_init(txPacket, NUM_PAD_BYTES, HDR_LEN, MAX_LENGTH);
    
            /* Zero out data in header before the length field */
            // for (int s = 0; s < LEN_INDEX; s++)
            // {
            //     txData[s] = 0U;
            // }
    
            /* Set the packet length */
            // txData[LEN_INDEX] = ble_pdu_send[0];
    
            memcpy(txData, ble_pdu_send, 17+1);
    
            /* Generate a random payload */
            // for (int i = HDR_LEN; i < MAX_LENGTH; i++)
            // {
            //     txData[i] = rand();
            // }
    
            /* Set packet to transmit */
            RCL_TxBuffer_put(&rclPacketTxCmdGenericTx.txBuffers, txPacket);
    
            rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle;
    
            /* Submit command */
            RCL_Command_submit(rclHandle, &rclPacketTxCmdGenericTx);
    
            /* Pend on command completion */
            RCL_Command_pend(&rclPacketTxCmdGenericTx);
    
            usleep(PACKET_INTERVAL);
        }
    }
    

    This is part of my test code, based on the original rfPacketTx example. I only made some simple packet construction changes and modified:

    #define FREQUENCY (2402000000U) // set to BLE channel 37
    

    I hope this helps clarify the issue I am trying to understand.

  • 你好,

    您应该查阅RCL API 指南中的BLE 命令处理程序(例如广播命令处理程序)和BLE5 文件参考。请注意,这需要使用自定义的 ti_radio_config.c/h 文件,因为 SysConfig 目前不支持自定义使用这些 RCL 命令。本质上,rfPacketTx 使用 BLE PHY,但并未公开所有 RCL 命令。您需要进一步研究文档,并尝试调整项目配置及其广播数据包结构,才能获得预期的输出。

    问候,
    瑞安

  • 您好:

    我已经能够成功发出了ble的广播包了,但是我的sniffer提示我:crc错误,但payload完整无误。但是我找不到在sysconfig当中设置他的地方,这些配置都被隐藏了吗。另外我使用的simplelink-lowpower-f3-sdk 8.10,我使用类似的代码在SDK 9.20上面是正确的,我找不到调试的方向,能否提供关于sysconfig配置Generic BLE的更多信息

  • 你好,

    您如何验证有效载荷是否完整?

    此致,

    塔雷克·D