This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2500EMK: 使用示例程序无法编译

Part Number: CC2500EMK
Other Parts Discussed in Thread: CC2500, MSP430F2274, MSP430F5529, SIMPLICITI

在下载了CC2500页面中的示例代码后使用CCS编译,但是会出现以下报错

"D:\\ccs\\utils\\bin\\gmake" -k all
 
Building target: "eZ430-RF2500_WSM.out"
Invoking: MSP430 Linker
"D:/ccs/tools/compiler/ti-cgt-msp430_20.2.4.LTS/bin/cl430" --cmd_file="C:/Users/WBL/Desktop/eZ430-RF2500 Wireless Sensor Monitor/Embedded/CCS/eZ430-RF2500_WSM/../Code/Configuration/smpl_nwk_config.dat" --cmd_file="C:/Users/WBL/Desktop/eZ430-RF2500 Wireless Sensor Monitor/Embedded/CCS/eZ430-RF2500_WSM/../Code/Configuration/smpl_config_ED.dat"  -vmsp -g -O3 --opt_for_speed=0 --define=__MSP430F2274__ --define=MRFI_CC2500 --diag_warning=225 --printf_support=minimal -z -m"eZ430-RF2500_WSM.map" --stack_size=80 --heap_size=80 --warn_sections -i"D:/ccs/ccs_base/msp430/include" -i"D:/ccs/tools/compiler/ti-cgt-msp430_20.2.4.LTS/lib" -i"D:/ccs/tools/compiler/ti-cgt-msp430_20.2.4.LTS/include" --reread_libs --xml_link_info="eZ430-RF2500_WSM_linkInfo.xml" --rom_model -o "eZ430-RF2500_WSM.out" "./Applications/main_ED.obj" "./Applications/vlo_rand.obj" "./Components/bsp/bsp.obj" "./Components/mrfi/mrfi.obj" "./Components/nwk/nwk.obj" "./Components/nwk/nwk_QMgmt.obj" "./Components/nwk/nwk_api.obj" "./Components/nwk/nwk_frame.obj" "./Components/nwk/nwk_globals.obj" "./Components/nwk_applications/nwk_freq.obj" "./Components/nwk_applications/nwk_ioctl.obj" "./Components/nwk_applications/nwk_join.obj" "./Components/nwk_applications/nwk_link.obj" "./Components/nwk_applications/nwk_mgmt.obj" "./Components/nwk_applications/nwk_ping.obj" "./Components/nwk_applications/nwk_security.obj" "../lnk_msp430f2274.cmd"  -lrts430.lib
<Linking>
error: cannot find file "rts430.lib"
"../lnk_msp430f2274.cmd", line 81: warning: Linker command file has no sections
   of type=VECT_INIT, but does contain .intXX sections.  This file may be out
   of date.  Generating interrupt pointers for all .intXX sections.  The
   default handler provided in the RTS will be used if no other handler is
   found.  It is recommend that you update your linker command file to the
   latest version.
warning: creating output section ".data" without a SECTIONS specification
warning: entry-point symbol "_c_int00" undefined
 
 undefined              first referenced          
  symbol                    in file               
 ---------              ----------------          
 __TI_decompress_lzss                             
 __TI_decompress_none                             
 __TI_int00                                       
 __TI_int01                                       
 __TI_int02                                       
 __TI_int04                                       
 __TI_int06                                       
 __TI_int07                                       
 __TI_int08                                       
 __TI_int10                                       
 __TI_int11                                       
 __TI_int12                                       
 __TI_int13                                       
 __TI_int14                                       
 __TI_zero_init                                   
 __mspabi_divi          ./Components/mrfi/mrfi.obj
 __mspabi_func_epilog_2 ./Components/mrfi/mrfi.obj
 __mspabi_func_epilog_3 ./Components/mrfi/mrfi.obj
 __mspabi_func_epilog_4 ./Components/nwk/nwk.obj  
 __mspabi_func_epilog_5 ./Components/nwk/nwk.obj  
 __mspabi_mpyi          ./Components/bsp/bsp.obj  
 __mspabi_srli_4        ./Components/mrfi/mrfi.obj
 memcmp                 ./Components/nwk/nwk.obj  
 memcpy                 ./Components/mrfi/mrfi.obj
 memmove                ./Components/nwk/nwk.obj  
 memset                 ./Components/mrfi/mrfi.obj
 
error: unresolved symbols remain
warning: no suitable entry-point found; setting to 0
error: errors encountered during linking; "eZ430-RF2500_WSM.out" not built
 
>> Compilation failure
makefile:159: recipe for target 'eZ430-RF2500_WSM.out' failed
gmake: *** [eZ430-RF2500_WSM.out] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

所以想请问一下是什么原因呢