This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: RF EASYLINK TX示例,改变payload类型

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650

TI工程师:

我使用了TI-RTOS for cc2650 - 2.21.00.06下的RF EASYLINK TX示例,在这个例子的“EasyLink.h”中定义了发送包的结构体,如下:

typedef struct
{
uint8_t dstAddr[8]; /// Dst Address
uint32_t absTime; ///Absolute time to Tx packet (0 for immediate)
///Layer will use last SeqNum used + 1
uint8_t len; ///Payload Length
uint8_t payload[EASYLINK_MAX_DATA_LENGTH]; ///Payload
} EasyLink_TxPacket;

当我运行示例时是成功的,但是当我把payload的类型从uint8_t改成uint32_t,我的开发板看起来不会发送数据了(因为LED1没有闪烁)。请问我应该如果传输数据类型为uint32_t的数据?

谢谢