This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: IQ数据处理遇到的疑惑

Part Number: LAUNCHXL-CC26X2R1

专家您好:

     我采用的是sdk5.30,3块cc2652和1块AOA-boostxl,进行搭载实验。

   配置是如下图1所示的,我采集到的IQ数据是:每个pkt 中的sample_idx采集180组(0-179),如下图2所示。这180组我理解的是:32+4*37

     

我将采集到的IQ数据分成天线1与天线2。sample1中有1us采样4个IQ数据,sample3采样的是天线1下一个4个IQ数据,这两个天线1的采样间隔了7us。然而按照载波250KHz的频率,载波周期为4us。那就是说天线1每4次采样的间隔是1.75个周期。如下图2所示,如果passive与responder角度保持不变的情况下,天线1采集的IQ数据是不是都是一样的(因为每次间隔7us)?但是,图3这个是天线1中的Q数据在图上画出来的点就不是一样的,反而有点呈现周期性变化。这是为什么?我哪里理解错了?