This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我这边为您提供了技术参考手册,您可以在12.14中找到相应的配置,主要去看一下CLKCON这部分的设置,我这边看您这边的代码,串口配置没什么问题,你这边是系统时钟的配置的问题,稍后我这边联系一下工程师,看一下外部时钟配置流程。您先查看一下datasheet。
CC2511 uses a 48 MHz Crystal:

数据表第12.1.5节显示,与CC2511一起使用的48 MHz XTAL被划分为24 MHz作为系统时钟。使用24 MHz时钟,可在表56中找到24 MHz的UART设置:
BAUD_E=12
BAUD_M=59
因此,BAUD_E=12和BAUD_M=216的上述设置不正确,导致波特率约为172851。