This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2500: CC2500问题描述

Part Number: CC2500


问题描述: Q3(为闪光灯,为我司的设计的产品),QPro-S(为引闪器,设计的产品).目前Q3和QPro-S都已经量产,并大批量出货. 目前是遭到客户投诉:Q3搭配QPro-S时,漏闪非常严重,大概100次有5次左右.而且能100%进行复现,而且是100%的机器都会搭配在一起时就会漏闪.但是搭配QPro-N以及QPro-C是不会漏闪. :Q3出货时,是有100%进行基带频率校准的.但是反馈我司的QPro-S是没有进行校准的.是需要对QPro-S 100%进行基带校准的. 我司的需求:基带校准方法,通过软件固化至产品中,产线出货时,固化基带频率,是的Q3与QPro-S的基带频率一致. 目前Q3的校准基带频率为2.412754GHz. 他们使用频谱仪:安捷伦E4404B进行测试基带频率.