This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A: EVM读取我自己基于RF430FRL152H设计的PCB时报错:IS015693 ROM Sensor Support Disabled

Part Number: TRF7970A
Other Parts Discussed in Thread: RF430FRL152H

我基于RF430FRL152H设计了一款面向NFC应用的PCB,并在ADC2 pin脚出连接了一个热敏电阻,想尝试验证一下NFC传输温度。我使用了官方下载的RF430FRL152HEVM GUI Windows,但是当我设置好一切,准备使用Demo Mode进行温度测量时,GUI报了错误:ISO15693 ROM Sensor Support Disabled,并且我点yes后也没有得到解决,而是不断跳出下面的弹窗。我想知道问题可能出现在什么地方?以及我应该怎么解决?